This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Kian,
Thank you for reaching out. I see that MCP1612 is a 1.4 MHz fixed switching frequency device.
If switching frequency is not a problem, then we have value line hero device with small solution size and similar package:
TPS62A01(PSM, high efficiency at light load conditions) and TPS62A01A (FPWM, 2.4 MHz Fixed frequency) with small solution size.
we also have another value line device TLV62568 with similar package, but the switching frequency is not fixed.
Please provide me the target efficiency and typical load condition and desired switching frequency and end application and any other special requirements. Based upon that I can suggest you a far better device compared to MCP1612.
Thank you,
Regards,
Moheddin.
Hi Moheddin,
Thanks for swift response. I don't have this specific demand about this device, it's just a multisource device.
Please provide me the target efficiency and typical load condition and desired switching frequency and end application and any other special requirements. Based upon that I can suggest you a far better device compared to MCP1612.
I think this hero product is much suitable.
TPS62A01A (FPWM, 2.4 MHz Fixed frequency) with small solution size
Thanks for your recommendation. If we show other requirement about this, I will reply under this thread.
BRs,
Kian
Hello Kian,
Please update me when you got more information.
Thank you,
Regards,
Moheddin.
Hi Moheddin,
Got that. If we have any progress, I will loop you over email.
Thanks.
BRs
Kian