This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: OTP fail

Part Number: BQ76952
Other Parts Discussed in Thread: BQSTUDIO,

hi sir,

I have imported the values from  a .gg file, and then finishing the  programe process to OTP memory.

after re-reading the RAM value, i found some of the values are not correct and some are right.

so I perform the programing process again,  and the values in OTP are totally right.

there are two question:

1)after the first programe process, why there are some values are not correct?

2) for this chip can only program in one time, so, in the second programe process, all these values are effected? 

thank you very much.