This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Bq27541 FlashData can't be written

Other Parts Discussed in Thread: BQ27541

4784.Bq27541 problem.docHi,

I am using Bq27541 for battery management.

But one problem i meet in production line.

When i want to write lot data into FlashData. it not works. (But almost all sample are fine)

The fail rate is lower (around 0.1%), but it do happen in few samples.

Note that IC was not sealed, and cell voltage is higher than [Flash updagte ok voltage]

But i can re-new DFI data by BqEASY.

Could somebody teach me what problem happened in IC?