This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R1:The difference between ASOC and RSOC

Part Number: BQ40Z50-R1

有客户投诉案例,客户反馈使用一年后电池寿命短,使用的电量计为40z50 R1,电池组为4S2P;读取电量计的ASOC和RSOC值,确定容量衰减了10%~12%,(重新测试老化机柜的容量发现损失在6%左右)判断是基于RSOC和ASOC在电量计中的差异,如下图所示。

问题:
1. ASOC在手册中没有解释,那么ASOC的详细定义是什么?什么是表达式,更新的机制是什么?
2. ASOC和RSOC有什么区别?实际应用中应注意什么?
3. 这种方法判断电池容量衰减可行吗?如果没有,有更好的建议吗?

寿命