Part Number: BQ24610
hi Team:
Recently, I encountered a problem when testing the BQ24610 battery charging EVM board with customer parameter. And the charging current does not reach the set value, Vsrp-Vsrn is less than 5mV, and the charging will stop automatically after 10 minutes of charging! Can you help to check what cause this issue ? tks!
setting parameter:
1.Charging current is set to 0.68A.
2.pre-charging current is 0.068A
3. input capacitor is 10μF
4. the output capacitor is 4.4μF
5. the inductance is 27μH
6.Input 24V, 5 lithium batteries, charging voltage 21V
result: The measured charging current is only 200mA, and the charging will stop after about 10 minutes.
here attached the waveform of Vbtst:

here attached the waveform of PH:

here attached the waveform of HIDRV:

here attached the waveform of LODRV: