Hi TI Teams,
Our customer feedback that when they setting the fast charge current to 500mA, but the measured output current in the constant voltage charging process is only 218mA. At this time, they have disable the wachdog.
The register setting is as below:
Addr | Value |
0x03 | 0x46 |
0x04 | 0x4D |
0x05 | 0x23 |
0x06 | 0x56 |
0x07 | 0x07 |
0x08 | 0x4D |
0x0A | 0x40 |
0x0B | 0x0F |
Other question is about the TS_EN. We disabled all the registers of the temperature setting, do we need to disable the TS_EN as well, otherwise the BQ25180 will not be able to work normally? That is, if we disabled all the registers of the temperature setting, but the TS_EN is enable, does the BQ25180 will stop charging when it fails to detect the temperature-related configuration?
Thanks,
Kind Regards