This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
Why is the efficiency of SOT-563 lower than SOT-235 under heavy load? Thanks.
Regards,
Charlie
Hello Charlie,
Thank you for reaching out.
The efficiency depends upon on many factors within different packages. such as junction temperature, RθJA etc.
In the case of TLV62569 SOT23-5 and TLV62569 SOT563. the difference in the efficiency is only ~ 0.1% to 0.2%. It is due to thermal performances, which is critical for higher load current as power dissipation becomes a challenge with conduction losses increasing.
I think you already have this app note - Thermal Comparison of a DC-DC Converter in SOT23 and the New SOT563 (Rev. A) (ti.com)
Thank you,
Regards,
Moheddin.