This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40210: trouble issue of the MOSFET over heating

Part Number: TPS40210


Hi Sir,

The customer is using the TPS40210 as a boost circuit(V-in=5V, V-out=48V, I-out 400mA).

The MOSFET over heating is derived from the customer changed the MOSFET from AOS / AOD2544 to CYStek / MTB050N15BRJ3.
When the boost system working after 5 mins, it was found that the MOSFET was seriously hot, and the temperature rose over 100°C (Vin=5V, V-out=48V, 200mA load).

Could you help analyze what the problem is?

They would like to know this problem is derived from MOSFET parameters or they miss to check other components parameter?


original MOSFET: AOS / AOD2544

AOD2544(normal part).pdf
alternative MOSFET: CYStek / MTB050N15BRJ3

MTB050N15BRJ3(abnormal part) .pdf

Schematic: