This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61161A: Output current under our conditions.

Guru 11295 points
Part Number: TPS61161A


Hi team,

I'd like to know if TPS61161A will work without problems in our conditions.
Based on the formula in the datasheet, it appears that 160 mA is the maximum output.
Since I plan to use 140mA output, is this a usable calculated value given the worst-case scenario?

*Conditions.
Vout : 25 V ( Typ 24V )
Vf : 0.6 V
Vin : 11.4 V ( Typ 12V )
Iout : 140mA

If not available, could you tell me about less expensive devices that can carry more current?
PWM control is a must.

Sincerely.
Kengo.