This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53626: About the TPS53626 IMON pin

Part Number: TPS53626

Please answer the following questions about the TPS53626 IMON pin.

1. The RIMON resistor is connected to the IMON pin. Is this constant related to the OCP current value (threshold)?
2. Is the IMON pin used only for monitoring the current value?
3. If the IMON pin is not used, what should be the resistance value of RIMON?