This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We did short circuit tests with our BMS and encountered a problem.
On some boards, the MOS-FET's are burnt approx. 1 second after the first short circuit.
Measured with an Ozillocop over 0.5mOhm you can see very clearly that the first short circuit is intercepted.
After about a second, the MOSFETs seem to be activated again.
However, the unlock delay is set to 10 seconds.
Is there another register set incorrectly?
Or how can the activation after approx. 1 second be avoided?
Hello Christian,
Can you share a BQStudio log of your tests so we can review the registers during the failure? Can you also share your .gg file with the full configuration for the test?
Sincerely,
Wyatt Keller
Tue Jan 24 11:49:47 CET 2023 Device Version Info = 4500_2_08 BQZ Device Name = bq40z50R2 BQZ Firmware Version = V2_08_BLD50 Design Capacity = 10500 Design Voltage = 12800 Specification Info = 0x0031 Manufacturer Date = 2022-9-15 Serial Number = 0x0001 Manufacturer Name = Device Name = Device Chemistry = LIFE Sample,DateTime,ElapsedTime,ManufAccess,RemCapAlarm,RemTimeAlarm,BattMode,@Rate(@),@TimeFull,@TimeEmpty,@RateOK,Temperature,Voltage,Current,AvgCurr,MaxErr,RSOC,ASOC,RemCap,FullChgCap,RunTimeEmty,AvgTimeEmty,AvgTimeFull,ChgCurr,ChgVolt,BattStat,CycleCnt,MaxTurboPwr,SusTurboPwr,MaxTurboCurr,SusTurboCurr,SoH,OpStatA,OpStatB,TempRange,ChgStat,GaugeStat,ITStat,MfgStat,SafetyAlertAB,SafetyStatAB,SafetyAlertCD,SafetyStatCD,PFAlertAB,PFStatAB,PFAlertCD,PFStatCD,CellVolt1,CellVolt2,CellVolt3,CellVolt4,vBAT,vPACK,CellCurr1,CellCurr2,CellCurr3,CellCurr4,CellPower1,CellPower2,CellPower3,CellPower4,Power,AvgPow,IntTemp,TS1Temp,TS2Temp,TS3Temp,TS4Temp,CellTemp,FETTemp,GaugeTemp,FltRemQ,FltRemE,FltFullChgQ,FltFullChgE,NoLoadRemCap,TrueRemQ,TrueRemE,InitialQ,InitialE,TrueFullChgQ,TrueFullChgE,T_sim,T_ambient,RaScale1,RaScale2,RaScale3,RaScale4,CompRes1,CompRes2,CompRes3,CompRes4,PackGrid,LStatus,CellGrid1,CellGrid2,CellGrid3,CellGrid4,StateTime,DOD0_1,DOD0_2,DOD0_3,DOD0_4,DOD0 Passed Q,DOD0 Passed E,DOD0 Time,DODEOC_1,DODEOC_2,DODEOC_3,DODEOC_4,QMax1,QMax2,QMax3,QMax4,QMaxDOD0_1,QMaxDOD0_2,QMaxDOD0_3,QMaxDOD0_4,QMaxPassedQ,QMaxTime,Tk,Ta,RawDOD_1,RawDOD_2,RawDOD_3,RawDOD_4,CBTime1,CBTime2,CBTime3,CBTime4,CBDOD_1,CBDOD_2,CBDOD_3,CBDOD_4,CBTotalDODChg,SOH_FC_Q,SOH_FC_E,LogRowTime(ms),LogStatus 1,2023-01-24 11:49:52,5.000,0x0187,300,10,0x6001,0,65535,65535,1,14.6,13952,0,0,1,99,108,11339,11454,65535,65535,65535,2500,14400,0x00C0,1,-32767,-23440,-32767,-21000,100,0x0187,0x0000,0x08,0x0008,0x50,0x0011,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3441,3507,3492,3512,13895,14038,0,0,0,0,0,0,0,0,0,0,15.8,14.6,14.9,15.0,-53.5,14.6,-273.2,14.6,11454,14420,11454,14420,11651,11454,14420,0,0,11454,14420,15.9,14.6,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,6880,0,0,0,0,0,0,30,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,30,1.17,860,0,0,0,0,0,0,0,0,0,0,0,0,16384,11527,14803,1196,SUCCESS 2,2023-01-24 11:49:57,10.001,0x0187,300,10,0x6001,0,65535,65535,1,14.5,13952,0,0,1,99,108,11339,11454,65535,65535,65535,2500,14400,0x00C0,1,-32767,-23440,-32767,-21000,100,0x0187,0x0000,0x08,0x0008,0x50,0x0011,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3441,3507,3492,3512,13894,14039,0,0,0,0,0,0,0,0,0,0,15.8,14.5,14.9,14.9,-53.3,14.5,-273.2,14.5,11454,14420,11454,14420,11651,11454,14420,0,0,11454,14420,15.9,14.5,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,6885,0,0,0,0,0,0,30,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,30,1.17,860,0,0,0,0,0,0,0,0,0,0,0,0,16384,11527,14803,1166,SUCCESS 3,2023-01-24 11:50:02,15.199,0x0187,300,10,0x6001,0,65535,65535,1,14.5,13952,0,0,1,99,108,11339,11454,65535,65535,65535,2500,14400,0x00C0,1,-32767,-23449,-32767,-21000,100,0x0187,0x0000,0x08,0x0008,0x50,0x0011,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3442,3507,3492,3512,13896,14038,0,0,0,0,0,0,0,0,0,0,15.8,14.5,14.9,14.9,-53.4,14.5,-273.2,14.5,11454,14420,11454,14420,11651,11454,14420,0,0,11454,14420,15.9,14.5,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,6890,0,0,0,0,0,0,30,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,30,1.17,860,0,0,0,0,0,0,0,0,0,0,0,0,16384,11527,14803,1232,SUCCESS 4,2023-01-24 11:50:07,20.002,0x0187,300,10,0x6001,0,65535,65535,1,14.5,13952,0,0,1,99,108,11339,11454,65535,65535,65535,2500,14400,0x00C0,1,-32767,-23449,-32767,-21000,100,0x0187,0x0000,0x08,0x0008,0x50,0x0011,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3441,3507,3492,3512,13896,14038,0,0,0,0,0,0,0,0,0,0,15.8,14.5,14.9,14.9,-53.5,14.5,-273.2,14.5,11454,14420,11454,14420,11651,11454,14420,0,0,11454,14420,15.9,14.5,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,6895,0,0,0,0,0,0,30,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,30,1.17,860,0,0,0,0,0,0,0,0,0,0,0,0,16384,11527,14803,1213,SUCCESS 5,2023-01-24 11:50:12,25.002,0x0187,300,10,0x6001,0,65535,65535,1,14.5,13952,0,0,1,99,108,11339,11454,65535,65535,65535,2500,14400,0x00C0,1,-32767,-23449,-32767,-21000,100,0x0187,0x0000,0x08,0x0008,0x50,0x0011,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3441,3507,3492,3512,13894,14040,0,0,0,0,0,0,0,0,0,0,15.8,14.5,14.8,14.9,-53.3,14.5,-273.2,14.5,11454,14420,11454,14420,11651,11454,14420,0,0,11454,14420,15.9,14.5,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,6900,0,0,0,0,0,0,30,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,30,1.17,860,0,0,0,0,0,0,0,0,0,0,0,0,16384,11527,14803,1243,SUCCESS 6,2023-01-24 11:50:17,30.003,0x0187,300,10,0x6001,0,65535,65535,1,14.5,13952,0,0,1,99,108,11339,11454,65535,65535,65535,2500,14400,0x00C0,1,-32767,-23449,-32767,-21000,100,0x0187,0x0000,0x08,0x0008,0x50,0x0011,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3441,3507,3492,3512,13895,14038,0,0,0,0,0,0,0,0,0,0,15.7,14.5,14.9,14.9,-53.4,14.5,-273.2,14.5,11454,14420,11454,14420,11651,11454,14420,0,0,11454,14420,15.9,14.5,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,6905,0,0,0,0,0,0,30,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,30,1.17,860,0,0,0,0,0,0,0,0,0,0,0,0,16384,11527,14803,1241,SUCCESS 7,2023-01-24 11:50:22,35.196,0x0187,300,10,0x6001,0,65535,65535,1,14.5,13952,0,0,1,99,108,11339,11454,65535,65535,65535,2500,14400,0x00C0,1,-32767,-23449,-32767,-21000,100,0x0187,0x0000,0x08,0x0008,0x50,0x0011,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3442,3507,3492,3512,13895,14039,0,0,0,0,0,0,0,0,0,0,15.7,14.5,14.8,14.9,-53.4,14.5,-273.2,14.5,11454,14420,11454,14420,11651,11454,14420,0,0,11454,14420,15.9,14.5,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,6910,0,0,0,0,0,0,30,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,30,1.17,860,0,0,0,0,0,0,0,0,0,0,0,0,16384,11527,14803,1220,SUCCESS 8,2023-01-24 11:50:27,40.004,0x0187,300,10,0x6001,0,65535,65535,1,14.5,13952,0,0,1,99,108,11339,11454,65535,65535,65535,2500,14400,0x00C0,1,-32767,-23449,-32767,-21000,100,0x0187,0x0000,0x08,0x0008,0x50,0x0011,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3441,3507,3492,3512,13895,14038,0,0,0,0,0,0,0,0,0,0,15.7,14.5,14.8,14.9,-53.4,14.5,-273.2,14.5,11454,14420,11454,14420,11651,11454,14420,0,0,11454,14420,15.9,14.5,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,6915,0,0,0,0,0,0,30,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,30,1.17,860,0,0,0,0,0,0,0,0,0,0,0,0,16384,11527,14803,1208,SUCCESS 9,2023-01-24 11:50:32,45.004,0x0187,300,10,0x6001,0,65535,65535,1,14.5,13952,0,0,1,99,108,11339,11454,65535,65535,65535,2500,14400,0x00C0,1,-32767,-23449,-32767,-21000,100,0x0187,0x0000,0x08,0x0008,0x50,0x0011,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3442,3507,3492,3512,13895,14038,0,0,0,0,0,0,0,0,0,0,15.7,14.5,14.8,14.9,-53.4,14.5,-273.2,14.5,11454,14420,11454,14420,11651,11454,14420,0,0,11454,14420,15.9,14.5,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,6920,0,0,0,0,0,0,30,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,30,1.17,860,0,0,0,0,0,0,0,0,0,0,0,0,16384,11527,14803,1255,SUCCESS 10,2023-01-24 11:50:37,50.005,0x0187,300,10,0x6001,0,65535,65535,1,14.5,13952,0,0,1,99,108,11339,11454,65535,65535,65535,2500,14400,0x00C0,1,-32767,-23449,-32767,-21000,100,0x0187,0x0000,0x08,0x0008,0x50,0x0011,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3441,3507,3492,3512,13895,14038,0,0,0,0,0,0,0,0,0,0,15.7,14.4,14.8,14.9,-53.3,14.4,-273.2,14.4,11454,14420,11454,14420,11651,11454,14420,0,0,11454,14420,15.9,14.4,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,6925,0,0,0,0,0,0,30,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,30,1.17,860,0,0,0,0,0,0,0,0,0,0,0,0,16384,11527,14803,1173,SUCCESS 11,2023-01-24 11:50:42,55.199,0x0187,300,10,0x6001,0,65535,65535,1,14.5,13952,0,0,1,99,108,11339,11454,65535,65535,65535,2500,14400,0x00C0,1,-32767,-23449,-32767,-21000,100,0x0187,0x0000,0x08,0x0008,0x50,0x0011,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3442,3507,3492,3512,13894,14039,0,0,0,0,0,0,0,0,0,0,15.7,14.4,14.8,14.9,-53.4,14.4,-273.2,14.4,11454,14420,11454,14420,11651,11454,14420,0,0,11454,14420,15.9,14.4,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,6930,0,0,0,0,0,0,30,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,30,1.17,860,0,0,0,0,0,0,0,0,0,0,0,0,16384,11527,14803,1231,SUCCESS 12,2023-01-24 11:50:47,60.006,0x0187,300,10,0x6001,0,65535,65535,1,14.4,13952,0,0,1,99,108,11339,11454,65535,65535,65535,2500,14400,0x00C0,1,-32767,-23449,-32767,-21000,100,0x0187,0x0000,0x08,0x0008,0x50,0x0011,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3441,3507,3492,3512,13893,14038,0,0,0,0,0,0,0,0,0,0,15.7,14.4,14.8,14.9,-53.5,14.4,-273.2,14.4,11454,14420,11454,14420,11651,11454,14420,0,0,11454,14420,15.9,14.4,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,6935,0,0,0,0,0,0,30,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,30,1.17,860,0,0,0,0,0,0,0,0,0,0,0,0,16384,11527,14803,1238,SUCCESS 13,2023-01-24 11:50:52,65.006,0x0187,300,10,0x6001,0,65535,65535,1,14.4,13952,0,0,1,99,108,11339,11454,65535,65535,65535,2500,14400,0x00C0,1,-32767,-23449,-32767,-21000,100,0x0187,0x0000,0x08,0x0008,0x50,0x0011,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3441,3507,3492,3512,13894,14038,0,0,0,0,0,0,0,0,0,0,15.7,14.4,14.8,14.8,-53.4,14.4,-273.2,14.4,11454,14420,11454,14420,11651,11454,14420,0,0,11454,14420,15.9,14.4,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,6940,0,0,0,0,0,0,30,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,30,1.17,860,0,0,0,0,0,0,0,0,0,0,0,0,16384,11527,14803,1223,SUCCESS 14,2023-01-24 11:50:57,70.006,0x0187,300,10,0x6001,0,65535,65535,1,14.4,13952,0,0,1,99,108,11339,11454,65535,65535,65535,2500,14400,0x00C0,1,-32767,-23449,-32767,-21000,100,0x0187,0x0000,0x08,0x0008,0x50,0x0011,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3441,3507,3492,3512,13895,14038,0,0,0,0,0,0,0,0,0,0,15.7,14.4,14.8,14.9,-53.3,14.4,-273.2,14.4,11454,14420,11454,14420,11651,11454,14420,0,0,11454,14420,15.9,14.4,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,6945,0,0,0,0,0,0,30,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,30,1.17,860,0,0,0,0,0,0,0,0,0,0,0,0,16384,11527,14803,1223,SUCCESS 15,2023-01-24 11:51:02,75.197,0x0187,300,10,0x6001,0,65535,65535,1,14.4,13952,0,0,1,99,108,11339,11454,65535,65535,65535,2500,14400,0x00C0,1,-32767,-23449,-32767,-21000,100,0x0187,0x0000,0x08,0x0008,0x50,0x0011,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3442,3507,3492,3512,13894,14039,0,0,0,0,0,0,0,0,0,0,15.7,14.4,14.8,14.8,-53.4,14.4,-273.2,14.4,11454,14420,11454,14420,11651,11454,14420,0,0,11454,14420,15.9,14.4,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,6950,0,0,0,0,0,0,30,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,30,1.17,860,0,0,0,0,0,0,0,0,0,0,0,0,16384,11527,14803,1205,SUCCESS 16,2023-01-24 11:51:07,80.007,0x0187,300,10,0x6001,0,65535,65535,1,14.4,13952,0,0,1,99,108,11339,11454,65535,65535,65535,2500,14400,0x00C0,1,-32767,-23449,-32767,-21000,100,0x0187,0x0000,0x08,0x0008,0x50,0x0011,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3441,3507,3492,3512,13894,14039,0,0,0,0,0,0,0,0,0,0,15.7,14.4,14.8,14.8,-53.5,14.4,-273.2,14.4,11454,14420,11454,14420,11651,11454,14420,0,0,11454,14420,15.9,14.4,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,6955,0,0,0,0,0,0,30,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,30,1.17,860,0,0,0,0,0,0,0,0,0,0,0,0,16384,11527,14803,1207,SUCCESS 17,2023-01-24 11:51:12,85.007,0x0187,300,10,0x6001,0,65535,65535,1,14.4,13952,0,0,1,99,108,11339,11454,65535,65535,65535,2500,14400,0x00C0,1,-32767,-23449,-32767,-21000,100,0x0187,0x0000,0x08,0x0008,0x50,0x0011,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3441,3507,3492,3512,13895,14038,0,0,0,0,0,0,0,0,0,0,15.7,14.4,14.8,14.8,-53.4,14.4,-273.2,14.4,11454,14420,11454,14420,11651,11454,14420,0,0,11454,14420,15.9,14.4,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,6960,0,0,0,0,0,0,30,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,30,1.17,860,0,0,0,0,0,0,0,0,0,0,0,0,16384,11527,14803,1239,SUCCESS 18,2023-01-24 11:51:17,90.007,0x0187,300,10,0x6001,0,65535,65535,1,14.4,13952,0,0,1,99,108,11339,11454,65535,65535,65535,2500,14400,0x00C0,1,-32767,-23449,-32767,-21000,100,0x0187,0x0000,0x08,0x0008,0x50,0x0011,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3441,3507,3492,3512,13895,14040,0,0,0,0,0,0,0,0,0,0,15.7,14.4,14.8,14.8,-53.4,14.4,-273.2,14.4,11454,14420,11454,14420,11651,11454,14420,0,0,11454,14420,15.9,14.4,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,6965,0,0,0,0,0,0,30,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,30,1.17,860,0,0,0,0,0,0,0,0,0,0,0,0,16384,11527,14803,1189,SUCCESS 19,2023-01-24 11:51:22,95.198,0x0187,300,10,0x6001,0,65535,65535,1,14.4,13952,0,0,1,99,108,11339,11454,65535,65535,65535,2500,14400,0x00C0,1,-32767,-23449,-32767,-21000,100,0x0187,0x0000,0x08,0x0008,0x50,0x0011,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3442,3507,3492,3512,13895,14038,0,0,0,0,0,0,0,0,0,0,15.6,14.4,14.8,14.8,-53.4,14.4,-273.2,14.4,11454,14420,11454,14420,11651,11454,14420,0,0,11454,14420,15.9,14.4,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,6970,0,0,0,0,0,0,30,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,30,1.17,860,0,0,0,0,0,0,0,0,0,0,0,0,16384,11527,14803,1234,SUCCESS 20,2023-01-24 11:51:27,100.008,0x0187,300,10,0x6001,0,65535,65535,1,14.4,13952,0,0,1,99,108,11339,11454,65535,65535,65535,2500,14400,0x00C0,1,-32767,-23449,-32767,-21000,100,0x0187,0x0000,0x08,0x0008,0x50,0x0011,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3441,3507,3492,3512,13895,14038,0,0,0,0,0,0,0,0,0,0,15.7,14.3,14.8,14.8,-53.4,14.4,-273.2,14.4,11454,14420,11454,14420,11651,11454,14420,0,0,11454,14420,15.9,14.3,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,6975,0,0,0,0,0,0,31,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,31,1.17,860,0,0,0,0,0,0,0,0,0,0,0,0,16384,11527,14803,1250,SUCCESS 21,2023-01-24 11:51:32,105.009,0x0187,300,10,0x6001,0,65535,65535,1,14.4,13952,0,0,1,99,108,11339,11454,65535,65535,65535,2500,14400,0x00C0,1,-32767,-23449,-32767,-21000,100,0x0187,0x0000,0x08,0x0008,0x50,0x0011,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3441,3507,3492,3512,13895,14039,0,0,0,0,0,0,0,0,0,0,15.6,14.4,14.8,14.8,-53.4,14.4,-273.2,14.4,11454,14420,11454,14420,11651,11454,14420,0,0,11454,14420,15.9,14.3,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,6980,0,0,0,0,0,0,31,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,31,1.17,860,0,0,0,0,0,0,0,0,0,0,0,0,16384,11527,14803,1219,SUCCESS 22,2023-01-24 11:51:37,110.009,0x0187,300,10,0x6001,0,65535,65535,1,14.3,13952,0,0,1,99,108,11339,11454,65535,65535,65535,2500,14400,0x00C0,1,-32767,-23449,-32767,-21000,100,0x0187,0x0000,0x08,0x0008,0x50,0x0011,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3441,3507,3492,3512,13894,14039,0,0,0,0,0,0,0,0,0,0,15.6,14.3,14.8,14.8,-53.5,14.3,-273.2,14.3,11454,14420,11454,14420,11651,11454,14420,0,0,11454,14420,15.9,14.3,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,6985,0,0,0,0,0,0,31,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,31,1.17,860,0,0,0,0,0,0,0,0,0,0,0,0,16384,11527,14803,1204,SUCCESS 23,2023-01-24 11:51:42,115.198,0x0187,300,10,0x6001,0,65535,65535,1,14.3,13952,0,0,1,99,108,11339,11454,65535,65535,65535,2500,14400,0x00C0,1,-32767,-23449,-32767,-21000,100,0x0187,0x0000,0x08,0x0008,0x50,0x0011,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3442,3507,3492,3512,13894,14038,0,0,0,0,0,0,0,0,0,0,15.6,14.3,14.7,14.8,-53.4,14.3,-273.2,14.3,11454,14420,11454,14420,11651,11454,14420,0,0,11454,14420,15.9,14.3,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,6990,0,0,0,0,0,0,31,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,31,1.17,860,0,0,0,0,0,0,0,0,0,0,0,0,16384,11527,14803,1250,SUCCESS 24,2023-01-24 11:51:47,120.010,0x0187,300,10,0x6001,0,65535,65535,1,14.3,13952,0,0,1,99,108,11339,11454,65535,65535,65535,2500,14400,0x00C0,1,-32767,-23449,-32767,-21000,100,0x0187,0x0000,0x08,0x0008,0x50,0x0011,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3441,3507,3492,3512,13894,14038,0,0,0,0,0,0,0,0,0,0,15.6,14.3,14.7,14.8,-53.4,14.3,-273.2,14.3,11454,14420,11454,14420,11651,11454,14420,0,0,11454,14420,15.9,14.3,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,6995,0,0,0,0,0,0,31,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,31,1.17,860,0,0,0,0,0,0,0,0,0,0,0,0,16384,11527,14803,1188,SUCCESS 25,2023-01-24 11:51:52,125.010,0x0187,300,10,0x6001,0,65535,65535,1,14.3,13952,0,0,1,99,108,11339,11454,65535,65535,65535,2500,14400,0x00C0,1,-32767,-23449,-32767,-21000,100,0x0187,0x0000,0x08,0x0008,0x50,0x0011,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3441,3507,3492,3512,13895,14038,0,0,0,0,0,0,0,0,0,0,15.6,14.3,14.7,14.8,-53.4,14.3,-273.2,14.3,11454,14420,11454,14420,11651,11454,14420,0,0,11454,14420,15.9,14.3,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,7000,0,0,0,0,0,0,31,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,31,1.17,860,0,0,0,0,0,0,0,0,0,0,0,0,16384,11527,14803,1186,SUCCESS 26,2023-01-24 11:51:57,130.010,0x0187,300,10,0x6001,0,65535,65535,1,14.3,13952,0,0,1,99,108,11339,11454,65535,65535,65535,2500,14400,0x00C0,1,-32767,-23449,-32767,-21000,100,0x0187,0x0000,0x08,0x0008,0x50,0x0011,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3441,3507,3492,3512,13894,14039,0,0,0,0,0,0,0,0,0,0,15.5,14.3,14.7,14.8,-53.4,14.3,-273.2,14.3,11454,14420,11454,14420,11651,11454,14420,0,0,11454,14420,15.9,14.3,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,7005,0,0,0,0,0,0,31,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,31,1.17,860,0,0,0,0,0,0,0,0,0,0,0,0,16384,11527,14803,1203,SUCCESS 27,2023-01-24 11:52:02,135.215,0x0181,300,10,0x6001,0,65535,65535,1,14.3,13946,-104,-104,1,99,108,11339,11454,65535,65535,65535,2500,14400,0x00C0,1,-32767,-23449,-32767,-21000,100,0x0181,0x0000,0x08,0x0008,0x40,0x0119,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,2953,2838,2799,3405,10119,542,-21719,-24575,-24575,-1124,-6414,-6974,-6879,-383,-6316,-145,15.6,14.5,14.8,17.1,-53.4,14.5,-273.2,14.5,11457,14404,11458,14406,11651,11457,14405,0,0,11458,14406,14.3,14.3,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,1,0,0,0,0,1,1,0,0,0,0,0,11658,11651,11668,11661,0,0,0,0,1,0,1.17,860,0,0,0,0,0,0,0,0,0,0,0,0,16384,11527,14803,1313,SUCCESS 28,2023-01-24 11:52:07,140.010,0x2985,300,10,0x6001,0,65535,65535,1,16.8,13757,0,0,1,99,109,11343,11458,65535,65535,65535,2500,14400,0x00C0,1,-32767,-23829,-32767,-21000,100,0x2985,0x0000,0x08,0x0008,0x50,0x0118,0x0298,0x0080,0x0040,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3413,3453,3441,3457,13707,13844,0,0,0,0,0,0,0,0,0,0,15.6,17.3,15.3,17.9,-53.5,16.9,-273.2,16.9,11457,14404,11458,14406,11650,11457,14405,0,0,11458,14406,14.3,14.3,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,3,0,0,0,0,1,1,0,0,0,0,0,11658,11651,11668,11661,0,0,0,0,1,0,1.17,860,0,0,0,0,0,0,0,0,0,0,0,0,16384,11527,14803,1286,SUCCESS 29,2023-01-24 11:52:12,145.011,0x0187,300,10,0x6001,0,65535,65535,1,18.7,13793,0,0,1,99,109,11343,11458,65535,65535,65535,2500,14400,0x00C0,1,-32767,-24135,-32767,-21000,100,0x0187,0x0000,0x08,0x0008,0x50,0x0118,0x0298,0x0080,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3419,3461,3450,3465,13742,13882,0,0,0,0,0,0,0,0,0,0,15.8,18.8,15.5,17.8,-53.4,18.7,-273.2,18.7,11457,14404,11458,14406,11650,11457,14405,0,0,11458,14406,14.3,14.3,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,8,0,0,0,0,1,1,0,0,0,0,0,11658,11651,11668,11661,0,0,0,0,1,0,1.17,860,0,0,0,0,0,0,0,0,0,0,0,0,16384,11527,14803,1287,SUCCESS 30,2023-01-24 11:52:17,150.011,0x0187,300,10,0x6001,0,65535,65535,1,19.1,13810,0,0,1,99,109,11343,11458,65535,65535,65535,2500,14400,0x00C0,1,-32767,-24274,-32767,-21000,100,0x0187,0x0000,0x08,0x0008,0x50,0x0118,0x0298,0x0080,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3422,3466,3455,3470,13755,13899,0,0,0,0,0,0,0,0,0,0,16.1,19.1,15.6,17.6,-53.3,19.1,-273.2,19.1,11457,14404,11458,14406,11650,11457,14405,0,0,11458,14406,14.3,14.3,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,13,0,0,0,0,1,1,0,0,0,0,0,11658,11651,11668,11661,0,0,0,0,1,0,1.17,860,0,0,0,0,0,0,0,0,0,0,0,0,16384,11527,14803,1270,SUCCESS 31,2023-01-24 11:52:22,155.215,0x0187,300,10,0x6001,0,65535,65535,1,19.0,13822,0,0,1,99,109,11343,11458,65535,65535,65535,2500,14400,0x00C0,1,-32767,-24274,-32767,-21000,100,0x0187,0x0000,0x08,0x0008,0x50,0x0118,0x0298,0x0080,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3425,3469,3458,3473,13768,13910,0,0,0,0,0,0,0,0,0,0,16.2,19.0,15.6,17.3,-53.4,19.0,-273.2,19.0,11457,14404,11458,14406,11650,11457,14405,0,0,11458,14406,14.3,14.3,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,18,0,0,0,0,1,1,0,0,0,0,0,11658,11651,11668,11661,0,0,0,0,1,0,1.17,860,0,0,0,0,0,0,0,0,0,0,0,0,16384,11527,14803,1300,SUCCESS 32,2023-01-24 11:52:27,160.012,0x0187,300,10,0x6001,0,65535,65535,1,19.0,13830,0,0,1,99,109,11343,11458,65535,65535,65535,2500,14400,0x00C0,1,-32767,-24253,-32767,-21000,100,0x0187,0x0000,0x08,0x0008,0x50,0x0118,0x0298,0x0080,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3425,3471,3460,3474,13776,13917,0,0,0,0,0,0,0,0,0,0,16.4,18.9,15.6,17.0,-53.5,19.0,-273.2,19.0,11457,14404,11458,14406,11650,11457,14405,0,0,11458,14406,14.3,14.3,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,23,0,0,0,0,1,1,0,0,0,0,0,11658,11651,11668,11661,0,0,0,0,1,0,1.17,860,0,0,0,0,0,0,0,0,0,0,0,0,16384,11527,14803,1269,SUCCESS 33,2023-01-24 11:52:32,165.012,0x0187,300,10,0x6001,0,65535,65535,1,18.9,13836,0,0,1,99,109,11343,11458,65535,65535,65535,2500,14400,0x00C0,1,-32767,-24188,-32767,-21000,100,0x0187,0x0000,0x08,0x0008,0x50,0x0118,0x0298,0x0080,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3426,3473,3461,3476,13781,13925,0,0,0,0,0,0,0,0,0,0,16.6,18.9,15.6,16.8,-53.3,18.9,-273.2,18.9,11457,14404,11458,14406,11650,11457,14405,0,0,11458,14406,14.3,14.3,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,28,0,0,0,0,1,1,0,0,0,0,0,11658,11651,11668,11661,0,0,0,0,1,0,1.17,860,0,0,0,0,0,0,0,0,0,0,0,0,16384,11527,14803,1268,SUCCESS 34,2023-01-24 11:52:37,170.012,0x0187,300,10,0x6001,0,65535,65535,1,18.8,13841,0,0,1,99,109,11343,11458,65535,65535,65535,2500,14400,0x00C0,1,-32767,-24188,-32767,-21000,100,0x0187,0x0000,0x08,0x0008,0x50,0x0118,0x0298,0x0080,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3427,3474,3463,3478,13786,13928,0,0,0,0,0,0,0,0,0,0,16.8,18.8,15.6,16.6,-53.4,18.8,-273.2,18.8,11457,14404,11458,14406,11650,11457,14405,0,0,11458,14406,14.3,14.3,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,33,0,0,0,0,1,1,0,0,0,0,0,11658,11651,11668,11661,0,0,0,0,1,0,1.17,860,0,0,0,0,0,0,0,0,0,0,0,0,16384,11527,14803,1239,SUCCESS 35,2023-01-24 11:52:42,175.215,0x0187,300,10,0x6001,0,65535,65535,1,18.7,13846,0,0,1,99,109,11343,11458,65535,65535,65535,2500,14400,0x00C0,1,-32767,-24146,-32767,-21000,100,0x0187,0x0000,0x08,0x0008,0x50,0x0118,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3428,3476,3464,3479,13792,13932,0,0,0,0,0,0,0,0,0,0,16.9,18.7,15.6,16.5,-53.3,18.7,-273.2,18.7,11457,14404,11458,14406,11650,11457,14405,0,0,11458,14406,14.3,14.3,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,38,0,0,0,0,1,1,0,0,0,0,0,11658,11651,11668,11661,0,0,0,0,1,0,1.17,860,0,0,0,0,0,0,0,0,0,0,0,0,16384,11527,14803,1256,SUCCESS 36,2023-01-24 11:52:47,180.013,0x0187,300,10,0x6001,0,65535,65535,1,18.6,13849,0,0,1,99,109,11343,11458,65535,65535,65535,2500,14400,0x00C0,1,-32767,-24146,-32767,-21000,100,0x0187,0x0000,0x08,0x0008,0x50,0x0118,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3428,3477,3465,3480,13796,13938,0,0,0,0,0,0,0,0,0,0,17.0,18.6,15.5,16.4,-53.3,18.6,-273.2,18.6,11457,14404,11458,14406,11650,11457,14405,0,0,11458,14406,14.3,14.3,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,43,0,0,0,0,1,1,0,0,0,0,0,11658,11651,11668,11661,0,0,0,0,1,0,1.17,860,0,0,0,0,0,0,0,0,0,0,0,0,16384,11527,14803,1267,SUCCESS 37,2023-01-24 11:52:52,185.013,0x0187,300,10,0x6001,0,65535,65535,1,18.6,13852,0,0,1,99,109,11343,11458,65535,65535,65535,2500,14400,0x00C0,1,-32767,-24135,-32767,-21000,100,0x0187,0x0000,0x08,0x0008,0x50,0x0118,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3428,3478,3466,3481,13798,13939,0,0,0,0,0,0,0,0,0,0,17.1,18.6,15.5,16.3,-53.4,18.6,-273.2,18.6,11457,14404,11458,14406,11650,11457,14405,0,0,11458,14406,14.3,14.3,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,48,0,0,0,0,1,1,0,0,0,0,0,11658,11651,11668,11661,0,0,0,0,1,0,1.17,860,0,0,0,0,0,0,0,0,0,0,0,0,16384,11527,14803,1267,SUCCESS 38,2023-01-24 11:52:57,190.013,0x0187,300,10,0x6001,0,65535,65535,1,18.5,13855,0,0,1,99,109,11343,11458,65535,65535,65535,2500,14400,0x00C0,1,-32767,-24135,-32767,-21000,100,0x0187,0x0000,0x08,0x0008,0x50,0x0118,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3429,3478,3467,3482,13801,13941,0,0,0,0,0,0,0,0,0,0,17.1,18.5,15.6,16.1,-53.4,18.5,-273.2,18.5,11457,14404,11458,14406,11650,11457,14405,0,0,11458,14406,14.3,14.3,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,53,0,0,0,0,1,1,0,0,0,0,0,11658,11651,11668,11661,0,0,0,0,1,0,1.17,860,0,0,0,0,0,0,0,0,0,0,0,0,16384,11527,14803,1365,SUCCESS
7268.bat_105Ah_v5.6_2023-01-24.gg.csv
Hello Christian,
The gauge will clear the ASCD when the firmware sees it (about one second interval) after the ASCD gets triggered multiple times in a row without clearing the counter then ASCDL should set and stop any more discharge until it is cleared (depending on the NR bit settings)
If you are testing with MOSFETs in parallel or large gate capacitance the gauge may not be able to pull the gate low fast enough to prevent FET damage. Can you share a snippet of your schematic?
Sincerely,
Wyatt Keller
Hello Wyatt,
There are 7 x IFRS7534-7PPBF parallel on the circuit.
Each Gate are connected paralell via 100 Ohm and over one 5,1k resitor to the DSG-Pin.
At BMS where the MOS-FET's don't burn out 1 sec after the short circuit,
this unlocking occurs again and again after approx. 1s.
NR = 1, ASCD:Latch Limit = 1, ASCD:Counter Dec Delay = 30s, ASCD:Recovery = 10s, ASCD:Reset = 120s.
Best regards
Christian Rump
Hello Christian,
The gauge may not be able to turn off all the FETs you have in parallel quick enough, you may need to add some external circuitry to pull down the gates faster. The battery monitor team has some useful collateral for this, let me know if this is useful: https://www.ti.com/lit/an/sluaa09a/sluaa09a.pdf?ts=1674691687604&ref_url=https%253A%252F%252Fwww.ti.com%252Fproduct%252FBQ76952
Sincerely,
Wyatt Keller
Hello Wyatt,
Thank you for the link to the document.
I've now tested some of this.
The MOS-FET's now survive the short circuit,
but it still seems to be activated after one second
and not after 10 seconds as set in the parameters.
Picture1: Short_200us_RVgate=47r+RVDSG=100r+Zener16V
CH2=DSG_Gate, CH1=Ishort over 0,5mOhm --> ~1kA
Picture2: Short_100ms_RVgate=47r+RVDSG=100r+Zener16V
CH2=DSG_Gate, CH1=Ishort over 0,5mOhm --> ~1kA
Picture3: Short_500ms_RVgate=100r+RVDSG=100r+Zener16V
CH1=Ishort over 0,5mOhm
Log of the last Test (see also Picture3):
Thu Feb 02 13:24:44 CET 2023 Device Version Info = 4500_2_08 BQZ Device Name = bq40z50R2 BQZ Firmware Version = V2_08_BLD50 Design Capacity = 10500 Design Voltage = 12800 Specification Info = 0x0031 Manufacturer Date = 2022-9-15 Serial Number = 0x0001 Manufacturer Name = Device Name = Device Chemistry = LIFE Sample,DateTime,ElapsedTime,ManufAccess,RemCapAlarm,RemTimeAlarm,BattMode,@Rate(@),@TimeFull,@TimeEmpty,@RateOK,Temperature,Voltage,Current,AvgCurr,MaxErr,RSOC,ASOC,RemCap,FullChgCap,RunTimeEmty,AvgTimeEmty,AvgTimeFull,ChgCurr,ChgVolt,BattStat,CycleCnt,MaxTurboPwr,SusTurboPwr,MaxTurboCurr,SusTurboCurr,SoH,OpStatA,OpStatB,TempRange,ChgStat,GaugeStat,ITStat,MfgStat,SafetyAlertAB,SafetyStatAB,SafetyAlertCD,SafetyStatCD,PFAlertAB,PFStatAB,PFAlertCD,PFStatCD,CellVolt1,CellVolt2,CellVolt3,CellVolt4,vBAT,vPACK,CellCurr1,CellCurr2,CellCurr3,CellCurr4,CellPower1,CellPower2,CellPower3,CellPower4,Power,AvgPow,IntTemp,TS1Temp,TS2Temp,TS3Temp,TS4Temp,CellTemp,FETTemp,GaugeTemp,FltRemQ,FltRemE,FltFullChgQ,FltFullChgE,NoLoadRemCap,TrueRemQ,TrueRemE,InitialQ,InitialE,TrueFullChgQ,TrueFullChgE,T_sim,T_ambient,RaScale1,RaScale2,RaScale3,RaScale4,CompRes1,CompRes2,CompRes3,CompRes4,PackGrid,LStatus,CellGrid1,CellGrid2,CellGrid3,CellGrid4,StateTime,DOD0_1,DOD0_2,DOD0_3,DOD0_4,DOD0 Passed Q,DOD0 Passed E,DOD0 Time,DODEOC_1,DODEOC_2,DODEOC_3,DODEOC_4,QMax1,QMax2,QMax3,QMax4,QMaxDOD0_1,QMaxDOD0_2,QMaxDOD0_3,QMaxDOD0_4,QMaxPassedQ,QMaxTime,Tk,Ta,RawDOD_1,RawDOD_2,RawDOD_3,RawDOD_4,CBTime1,CBTime2,CBTime3,CBTime4,CBDOD_1,CBDOD_2,CBDOD_3,CBDOD_4,CBTotalDODChg,SOH_FC_Q,SOH_FC_E,LogRowTime(ms),LogStatus 1,2023-02-02 13:24:50,5.002,0x0107,300,10,0x6001,0,65535,65535,1,19.1,13341,0,0,1,97,105,10928,11372,65535,65535,65535,2500,14400,0x00C0,1,-32767,-23932,-32767,-21000,100,0x0107,0x0000,0x08,0x0008,0x50,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3330,3336,3335,3340,13379,13435,0,0,0,0,0,0,0,0,0,0,19.8,19.1,19.4,19.5,-53.4,19.1,-273.2,19.1,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,18.9,18.8,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,165,832,696,704,624,0,0,0,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,0,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1296,SUCCESS 2,2023-02-02 13:24:55,10.001,0x0107,300,10,0x6001,0,65535,65535,1,19.1,13341,0,0,1,97,105,10928,11372,65535,65535,65535,2500,14400,0x00C0,1,-32767,-23932,-32767,-21000,100,0x0107,0x0000,0x08,0x0008,0x50,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3330,3336,3335,3340,13379,13436,0,0,0,0,0,0,0,0,0,0,19.8,19.1,19.4,19.5,-53.4,19.1,-273.2,19.1,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,18.9,18.8,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,170,832,696,704,624,0,0,0,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,0,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1299,SUCCESS 3,2023-02-02 13:25:00,15.281,0x0107,300,10,0x6001,0,65535,65535,1,19.1,13341,0,0,1,97,105,10928,11372,65535,65535,65535,2500,14400,0x00C0,1,-32767,-23932,-32767,-21000,100,0x0107,0x0000,0x08,0x0008,0x50,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3332,3336,3335,3341,13380,13435,0,0,0,0,0,0,0,0,0,0,19.8,19.1,19.4,19.5,-53.5,19.1,-273.2,19.1,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,18.9,18.8,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,175,832,696,704,624,0,0,0,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,0,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1267,SUCCESS 4,2023-02-02 13:25:05,20.001,0x0107,300,10,0x6001,0,65535,65535,1,19.1,13341,0,0,1,97,105,10928,11372,65535,65535,65535,2500,14400,0x00C0,1,-32767,-23932,-32767,-21000,100,0x0107,0x0000,0x08,0x0008,0x50,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3330,3335,3335,3341,13379,13436,0,0,0,0,0,0,0,0,0,0,19.7,19.1,19.4,19.5,-53.3,19.1,-273.2,19.1,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,18.9,18.8,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,180,832,696,704,624,0,0,0,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,0,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1250,SUCCESS 5,2023-02-02 13:25:10,25.015,0x0107,300,10,0x6001,0,65535,65535,1,19.1,13341,0,0,1,97,105,10928,11372,65535,65535,65535,2500,14400,0x00C0,1,-32767,-23932,-32767,-21000,100,0x0107,0x0000,0x08,0x0008,0x50,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3330,3335,3335,3340,13381,13434,0,0,0,0,0,0,0,0,0,0,19.7,19.1,19.4,19.5,-53.3,19.1,-273.2,19.1,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,18.9,18.8,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,185,832,696,704,624,0,0,0,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,0,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1267,SUCCESS 6,2023-02-02 13:25:15,30.028,0x0107,300,10,0x6001,0,65535,65535,1,19.1,13341,0,0,1,97,105,10928,11372,65535,65535,65535,2500,14400,0x00C0,1,-32767,-23932,-32767,-21000,100,0x0107,0x0000,0x08,0x0008,0x50,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3330,3335,3335,3341,13380,13437,0,0,0,0,0,0,0,0,0,0,19.8,19.1,19.4,19.5,-53.3,19.1,-273.2,19.1,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,18.9,18.8,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,190,832,696,704,624,0,0,0,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,0,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1254,SUCCESS 7,2023-02-02 13:25:20,35.280,0x0107,300,10,0x6001,0,65535,65535,1,19.1,13341,0,0,1,97,105,10928,11372,65535,65535,65535,2500,14400,0x00C0,1,-32767,-23932,-32767,-21000,100,0x0107,0x0000,0x08,0x0008,0x50,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3332,3336,3335,3341,13379,13437,0,0,0,0,0,0,0,0,0,0,19.8,19.1,19.4,19.5,-53.5,19.1,-273.2,19.1,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,18.9,18.8,1000,1000,1000,1000,0,0,0,0,0,14,0,0,0,0,195,832,696,704,624,0,0,0,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,0,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1249,SUCCESS 8,2023-02-02 13:25:25,40.045,0x0101,300,10,0x6001,0,65535,65535,1,19.1,13337,-58,-48,1,97,105,10928,11372,13951,13660,65535,2500,14400,0x00C0,1,-32767,-23990,-32767,-21000,100,0x0101,0x0000,0x08,0x0008,0x40,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3330,3335,3334,3340,13381,22,-16,2,3,-10,-5,1,1,-3,-79,-65,19.8,19.1,19.4,19.5,-53.4,19.1,-273.2,19.1,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,19.1,18.8,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,2,832,696,704,624,0,0,0,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,0,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1297,SUCCESS 9,2023-02-02 13:25:30,45.045,0x0107,300,10,0x6001,0,65535,65535,1,19.2,13342,0,0,1,97,105,10928,11372,65535,65535,65535,2500,14400,0x00C0,1,-32767,-23932,-32767,-21000,100,0x0107,0x0000,0x08,0x0008,0x50,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3330,3336,3335,3341,13379,13437,0,0,0,0,0,0,0,0,0,0,19.8,19.2,19.4,19.5,-53.4,19.2,-273.2,19.2,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,19.1,18.8,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,4,832,696,704,624,0,0,0,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,0,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1254,SUCCESS 10,2023-02-02 13:25:35,50.061,0x0107,300,10,0x6001,0,65535,65535,1,19.2,13342,0,0,1,97,105,10928,11372,65535,65535,65535,2500,14400,0x00C0,1,-32767,-23932,-32767,-21000,100,0x0107,0x0000,0x08,0x0008,0x50,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3330,3336,3335,3341,13379,13436,0,0,0,0,0,0,0,0,0,0,19.7,19.2,19.4,19.5,-53.5,19.2,-273.2,19.2,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,19.1,18.8,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,9,832,696,704,624,0,0,0,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,0,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1283,SUCCESS 11,2023-02-02 13:25:40,55.309,0x0107,300,10,0x6001,0,65535,65535,1,19.2,13341,0,0,1,97,105,10928,11372,65535,65535,65535,2500,14400,0x00C0,1,-32767,-23932,-32767,-21000,100,0x0107,0x0000,0x08,0x0008,0x50,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3332,3336,3335,3340,13379,13434,0,0,0,0,0,0,0,0,0,0,19.8,19.2,19.4,19.5,-53.3,19.2,-273.2,19.2,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,19.1,18.8,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,14,832,696,704,624,0,0,0,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,0,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1269,SUCCESS 12,2023-02-02 13:25:45,60.078,0x0107,300,10,0x6001,0,65535,65535,1,19.2,13342,0,0,1,97,105,10928,11372,65535,65535,65535,2500,14400,0x00C0,1,-32767,-23932,-32767,-21000,100,0x0107,0x0000,0x08,0x0008,0x50,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3330,3336,3335,3341,13380,13437,0,0,0,0,0,0,0,0,0,0,19.7,19.2,19.4,19.4,-53.5,19.2,-273.2,19.2,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,19.1,18.8,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,19,832,696,704,624,0,0,0,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,0,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1266,SUCCESS 13,2023-02-02 13:25:50,65.094,0x0107,300,10,0x6001,0,65535,65535,1,19.2,13343,0,0,1,97,105,10928,11372,65535,65535,65535,2500,14400,0x00C0,1,-32767,-23932,-32767,-21000,100,0x0107,0x0000,0x08,0x0008,0x50,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3330,3335,3335,3340,13379,13436,0,0,0,0,0,0,0,0,0,0,19.8,19.2,19.4,19.4,-53.3,19.2,-273.2,19.2,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,19.1,18.8,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,24,832,696,704,624,0,0,1,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,1,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1220,SUCCESS 14,2023-02-02 13:25:55,70.006,0x0107,300,10,0x6001,0,65535,65535,1,19.2,13343,0,0,1,97,105,10928,11372,65535,65535,65535,2500,14400,0x00C0,1,-32767,-23932,-32767,-21000,100,0x0107,0x0000,0x08,0x0008,0x50,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3330,3336,3335,3340,13380,13436,0,0,0,0,0,0,0,0,0,0,19.7,19.2,19.4,19.4,-53.4,19.2,-273.2,19.2,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,19.1,18.8,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,29,832,696,704,624,0,0,1,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,1,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1260,SUCCESS 15,2023-02-02 13:26:00,75.249,0x0101,300,10,0x6001,0,65535,65535,1,19.2,13337,-58,-48,1,97,105,10928,11372,13660,13660,65535,2500,14400,0x00C0,1,-32767,-23990,-32767,-21000,100,0x0101,0x0000,0x08,0x0008,0x40,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3330,3335,3335,3340,13379,23,-15,4,2,-5,-5,1,1,-2,-77,-65,19.9,19.2,19.4,19.4,-53.3,19.2,-273.2,19.2,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,19.2,18.8,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,2,832,696,704,624,0,0,1,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,1,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1309,SUCCESS 16,2023-02-02 13:26:05,80.008,0x0107,300,10,0x6001,0,65535,65535,1,19.3,13342,0,0,1,97,105,10928,11372,65535,65535,65535,2500,14400,0x00C0,1,-32767,-23976,-32767,-21000,100,0x0107,0x0000,0x08,0x0008,0x50,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3330,3335,3335,3340,13379,13434,0,0,0,0,0,0,0,0,0,0,19.8,19.3,19.4,19.4,-53.4,19.3,-273.2,19.3,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,19.2,18.8,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,3,832,696,704,624,0,0,1,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,1,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1212,SUCCESS 17,2023-02-02 13:26:10,85.008,0x0107,300,10,0x6001,0,65535,65535,1,19.4,13342,0,0,1,97,105,10928,11372,65535,65535,65535,2500,14400,0x00C0,1,-32767,-24007,-32767,-21000,100,0x0107,0x0000,0x08,0x0008,0x50,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3330,3335,3334,3340,13379,13437,0,0,0,0,0,0,0,0,0,0,19.7,19.4,19.4,19.4,-53.4,19.4,-273.2,19.4,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,19.2,18.8,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,8,832,696,704,624,0,0,1,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,1,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1225,SUCCESS 18,2023-02-02 13:26:15,90.008,0x0107,300,10,0x6001,0,65535,65535,1,19.4,13342,0,0,1,97,105,10928,11372,65535,65535,65535,2500,14400,0x00C0,1,-32767,-24007,-32767,-21000,100,0x0107,0x0000,0x08,0x0008,0x50,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3330,3335,3335,3340,13378,13435,0,0,0,0,0,0,0,0,0,0,19.8,19.4,19.4,19.4,-53.4,19.4,-273.2,19.4,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,19.2,18.8,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,13,832,696,704,624,0,0,1,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,1,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1179,SUCCESS 19,2023-02-02 13:26:20,95.295,0x0107,300,10,0x6001,0,65535,65535,1,19.4,13341,0,0,1,97,105,10928,11372,65535,65535,65535,2500,14400,0x00C0,1,-32767,-24007,-32767,-21000,100,0x0107,0x0000,0x08,0x0008,0x50,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3330,3335,3335,3340,13379,13436,0,0,0,0,0,0,0,0,0,0,19.8,19.4,19.4,19.4,-53.3,19.4,-273.2,19.4,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,19.2,18.8,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,18,832,696,704,624,0,0,1,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,1,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1187,SUCCESS 20,2023-02-02 13:26:25,100.009,0x0107,300,10,0x6001,0,65535,65535,1,19.4,13342,0,0,1,97,105,10928,11372,65535,65535,65535,2500,14400,0x00C0,1,-32767,-24007,-32767,-21000,100,0x0107,0x0000,0x08,0x0008,0x50,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3330,3336,3335,3340,13379,13435,0,0,0,0,0,0,0,0,0,0,19.8,19.4,19.4,19.4,-53.5,19.4,-273.2,19.4,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,19.2,18.8,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,23,832,696,704,624,0,0,1,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,1,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1209,SUCCESS 21,2023-02-02 13:26:30,105.010,0x0107,300,10,0x6001,0,65535,65535,1,19.4,13341,0,0,1,97,105,10928,11372,65535,65535,65535,2500,14400,0x00C0,1,-32767,-24007,-32767,-21000,100,0x0107,0x0000,0x08,0x0008,0x50,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3330,3335,3335,3340,13379,13434,0,0,0,0,0,0,0,0,0,0,19.8,19.4,19.4,19.4,-53.4,19.4,-273.2,19.4,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,19.2,18.8,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,28,832,696,704,624,0,0,1,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,1,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1208,SUCCESS 22,2023-02-02 13:26:35,110.010,0x0107,300,10,0x6001,0,65535,65535,1,19.4,13341,0,0,1,97,105,10928,11372,65535,65535,65535,2500,14400,0x00C0,1,-32767,-24007,-32767,-21000,100,0x0107,0x0000,0x08,0x0008,0x50,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3330,3335,3335,3341,13379,13435,0,0,0,0,0,0,0,0,0,0,19.8,19.4,19.4,19.4,-53.3,19.4,-273.2,19.4,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,19.2,18.8,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,33,832,696,704,624,0,0,1,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,1,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1273,SUCCESS 23,2023-02-02 13:26:40,115.297,0x0107,300,10,0x6001,0,65535,65535,1,19.4,13340,0,0,1,97,105,10928,11372,65535,65535,65535,2500,14400,0x00C0,1,-32767,-24007,-32767,-21000,100,0x0107,0x0000,0x08,0x0008,0x50,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3330,3336,3335,3340,13380,13434,0,0,0,0,0,0,0,0,0,0,19.8,19.4,19.3,19.4,-53.4,19.4,-273.2,19.4,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,19.2,18.8,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,38,832,696,704,624,0,0,1,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,1,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1250,SUCCESS 24,2023-02-02 13:26:45,120.011,0x0107,300,10,0x6001,0,65535,65535,1,19.4,13340,0,0,1,97,105,10928,11372,65535,65535,65535,2500,14400,0x00C0,1,-32767,-24007,-32767,-21000,100,0x0107,0x0000,0x08,0x0008,0x50,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3330,3335,3335,3340,13379,13434,0,0,0,0,0,0,0,0,0,0,19.8,19.4,19.4,19.4,-53.5,19.4,-273.2,19.4,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,19.2,18.8,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,43,832,696,704,624,0,0,1,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,1,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1223,SUCCESS 25,2023-02-02 13:26:50,125.012,0x0107,300,10,0x6001,0,65535,65535,1,19.4,13340,0,0,1,97,105,10928,11372,65535,65535,65535,2500,14400,0x00C0,1,-32767,-24007,-32767,-21000,100,0x0107,0x0000,0x08,0x0008,0x50,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3330,3336,3335,3340,13379,13436,0,0,0,0,0,0,0,0,0,0,19.8,19.4,19.4,19.4,-53.4,19.4,-273.2,19.4,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,19.2,18.8,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,48,832,696,704,624,0,0,1,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,1,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1237,SUCCESS 26,2023-02-02 13:26:55,130.012,0x0107,300,10,0x6001,0,65535,65535,1,19.4,13340,0,0,1,97,105,10928,11372,65535,65535,65535,2500,14400,0x00C0,1,-32767,-24007,-32767,-21000,100,0x0107,0x0000,0x08,0x0008,0x50,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3330,3335,3335,3340,13379,13434,0,0,0,0,0,0,0,0,0,0,19.8,19.4,19.4,19.3,-53.5,19.4,-273.2,19.4,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,19.2,18.8,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,53,832,696,704,624,0,0,1,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,1,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1206,SUCCESS 27,2023-02-02 13:27:00,135.294,0x0107,300,10,0x6001,0,65535,65535,1,19.4,13342,0,0,1,97,105,10928,11372,65535,65535,65535,2500,14400,0x00C0,1,-32767,-24007,-32767,-21000,100,0x0107,0x0000,0x08,0x0008,0x50,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3330,3336,3335,3340,13381,13437,0,0,0,0,0,0,0,0,0,0,19.8,19.4,19.3,19.3,-53.5,19.4,-273.2,19.4,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,19.2,18.8,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,58,832,696,704,624,0,0,1,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,1,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1205,SUCCESS 28,2023-02-02 13:27:05,140.014,0x0107,300,10,0x6001,0,65535,65535,1,19.4,13340,0,0,1,97,105,10928,11372,65535,65535,65535,2500,14400,0x00C0,1,-32767,-24007,-32767,-21000,100,0x0107,0x0000,0x08,0x0008,0x50,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3330,3336,3335,3340,13379,13436,0,0,0,0,0,0,0,0,0,0,19.9,19.4,19.4,19.3,-53.4,19.4,-273.2,19.4,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,19.2,18.8,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,63,832,696,704,624,0,0,1,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,1,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1235,SUCCESS 29,2023-02-02 13:27:10,145.014,0x0107,300,10,0x6001,0,65535,65535,1,19.4,13339,0,0,1,97,105,10928,11372,65535,65535,65535,2500,14400,0x00C0,1,-32767,-24007,-32767,-21000,100,0x0107,0x0000,0x08,0x0008,0x50,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3330,3336,3335,3340,13380,13436,0,0,0,0,0,0,0,0,0,0,19.8,19.4,19.4,19.3,-53.4,19.4,-273.2,19.4,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,19.2,18.8,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,68,832,696,704,624,0,0,1,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,1,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1250,SUCCESS 30,2023-02-02 13:27:15,150.015,0x0107,300,10,0x6001,0,65535,65535,1,19.4,13340,0,0,1,97,105,10928,11372,65535,65535,65535,2500,14400,0x00C0,1,-32767,-24007,-32767,-21000,100,0x0107,0x0000,0x08,0x0008,0x50,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3330,3336,3335,3340,13379,13435,0,0,0,0,0,0,0,0,0,0,19.9,19.4,19.3,19.3,-53.5,19.4,-273.2,19.4,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,19.2,18.8,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,72,832,696,704,624,0,0,1,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,1,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1249,SUCCESS 31,2023-02-02 13:27:20,155.296,0x0107,300,10,0x6001,0,65535,65535,1,19.4,13342,0,-49,1,97,105,10928,11372,11503,13381,65535,2500,14400,0x00C0,1,-32767,-24068,-32767,-21000,100,0x0107,0x0000,0x08,0x0008,0x40,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3330,3335,3335,3340,13379,12909,0,0,0,0,0,0,0,0,0,-66,19.9,19.4,19.4,19.4,-53.3,19.4,-273.2,19.4,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,19.4,18.8,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,0,832,696,704,624,0,0,1,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,1,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1220,SUCCESS 32,2023-02-02 13:27:25,160.017,0x0107,300,10,0x6001,0,65535,65535,1,19.4,13340,0,0,1,97,105,10928,11372,65535,65535,65535,2500,14400,0x00C0,1,-32767,-24007,-32767,-21000,100,0x0107,0x0000,0x08,0x0008,0x50,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3330,3336,3334,3340,13378,13434,0,0,0,0,0,0,0,0,0,0,19.9,19.4,19.3,19.4,-53.4,19.4,-273.2,19.4,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,19.4,18.8,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,4,832,696,704,624,0,0,1,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,1,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1261,SUCCESS 33,2023-02-02 13:27:30,165.031,0x0107,300,10,0x6001,0,65535,65535,1,19.5,13340,0,0,1,97,105,10928,11372,65535,65535,65535,2500,14400,0x00C0,1,-32767,-24018,-32767,-21000,100,0x0107,0x0000,0x08,0x0008,0x50,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3330,3335,3335,3340,13379,13434,0,0,0,0,0,0,0,0,0,0,19.9,19.5,19.4,19.4,-53.4,19.5,-273.2,19.5,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,19.4,18.8,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,9,832,696,704,624,0,0,1,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,1,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1236,SUCCESS 34,2023-02-02 13:27:35,170.046,0x0107,300,10,0x6001,0,65535,65535,1,19.5,13340,0,0,1,97,105,10928,11372,65535,65535,65535,2500,14400,0x00C0,1,-32767,-24018,-32767,-21000,100,0x0107,0x0000,0x08,0x0008,0x50,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3330,3335,3335,3340,13380,13436,0,0,0,0,0,0,0,0,0,0,19.9,19.5,19.3,19.4,-53.5,19.5,-273.2,19.5,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,19.4,18.8,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,14,832,696,704,624,0,0,1,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,1,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1219,SUCCESS 35,2023-02-02 13:27:40,175.296,0x0107,300,10,0x6001,0,65535,65535,1,19.5,13342,0,0,1,97,105,10928,11372,65535,65535,65535,2500,14400,0x00C0,1,-32767,-24018,-32767,-21000,100,0x0107,0x0000,0x08,0x0008,0x50,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3330,3336,3335,3340,13378,13434,0,0,0,0,0,0,0,0,0,0,19.8,19.5,19.3,19.3,-53.5,19.5,-273.2,19.5,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,19.4,18.8,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,20,832,696,704,624,0,0,1,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,1,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1252,SUCCESS 36,2023-02-02 13:27:45,180.060,0x0107,300,10,0x6001,0,65535,65535,1,19.5,13340,0,0,1,97,105,10928,11372,65535,65535,65535,2500,14400,0x00C0,1,-32767,-24018,-32767,-21000,100,0x0107,0x0000,0x08,0x0008,0x50,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3330,3335,3335,3340,13380,13434,0,0,0,0,0,0,0,0,0,0,19.9,19.5,19.3,19.3,-53.3,19.5,-273.2,19.5,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,19.4,18.8,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,24,832,696,704,624,0,0,1,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,1,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1238,SUCCESS 37,2023-02-02 13:27:50,185.063,0x0107,300,10,0x6001,0,65535,65535,1,19.5,13340,0,0,1,97,105,10928,11372,65535,65535,65535,2500,14400,0x00C0,1,-32767,-24018,-32767,-21000,100,0x0107,0x0000,0x08,0x0008,0x50,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3330,3335,3335,3340,13379,13437,0,0,0,0,0,0,0,0,0,0,19.9,19.5,19.4,19.4,-53.3,19.5,-273.2,19.5,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,19.4,18.8,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,29,832,696,704,624,0,0,1,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,1,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1203,SUCCESS 38,2023-02-02 13:27:55,190.077,0x0107,300,10,0x6001,0,65535,65535,1,19.5,13340,0,0,1,97,105,10928,11372,65535,65535,65535,2500,14400,0x00C0,1,-32767,-24018,-32767,-21000,100,0x0107,0x0000,0x08,0x0008,0x50,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3330,3335,3335,3340,13378,13436,0,0,0,0,0,0,0,0,0,0,19.9,19.5,19.3,19.3,-53.4,19.5,-273.2,19.5,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,19.4,18.8,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,34,832,696,704,624,0,0,1,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,1,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1235,SUCCESS 39,2023-02-02 13:28:00,195.328,0x0107,300,10,0x6001,0,65535,65535,1,19.5,13342,0,0,1,97,105,10928,11372,65535,65535,65535,2500,14400,0x00C0,1,-32767,-24018,-32767,-21000,100,0x0107,0x0000,0x08,0x0008,0x50,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3330,3335,3334,3340,13379,13414,0,0,0,0,0,0,0,0,0,0,19.9,19.5,19.3,19.4,-53.4,19.5,-273.2,19.5,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,19.5,18.8,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,1,832,696,704,624,0,0,1,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,1,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1233,SUCCESS 40,2023-02-02 13:28:05,200.093,0x0107,300,10,0x6001,0,65535,65535,1,19.5,13340,0,0,1,97,105,10928,11372,65535,65535,65535,2500,14400,0x00C0,1,-32767,-24018,-32767,-21000,100,0x0107,0x0000,0x08,0x0008,0x50,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3330,3335,3335,3340,13378,13436,0,0,0,0,0,0,0,0,0,0,19.9,19.5,19.4,19.3,-53.4,19.5,-273.2,19.5,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,19.5,18.8,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,5,832,696,704,624,0,0,1,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,1,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1220,SUCCESS 41,2023-02-02 13:28:10,205.110,0x0107,300,10,0x6001,0,65535,65535,1,19.5,13341,0,0,1,97,105,10928,11372,65535,65535,65535,2500,14400,0x00C0,1,-32767,-24018,-32767,-21000,100,0x0107,0x0000,0x08,0x0008,0x50,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3330,3335,3335,3340,13378,13436,0,0,0,0,0,0,0,0,0,0,19.9,19.5,19.4,19.3,-53.5,19.5,-273.2,19.5,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,19.5,18.8,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,10,832,696,704,624,0,0,1,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,1,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1265,SUCCESS 42,2023-02-02 13:28:15,210.109,0x0107,300,10,0x6001,0,65535,65535,1,19.5,13340,0,0,1,97,105,10928,11372,65535,65535,65535,2500,14400,0x00C0,1,-32767,-24018,-32767,-21000,100,0x0107,0x0000,0x08,0x0008,0x50,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3330,3335,3335,3341,13379,13434,0,0,0,0,0,0,0,0,0,0,19.9,19.5,19.3,19.3,-53.4,19.5,-273.2,19.5,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,19.5,18.8,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,15,832,696,704,624,0,0,1,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,1,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1205,SUCCESS 43,2023-02-02 13:28:20,215.263,0x0107,300,10,0x6001,0,65535,65535,1,19.5,13340,0,0,1,97,105,10928,11372,65535,65535,65535,2500,14400,0x00C0,1,-32767,-24018,-32767,-21000,100,0x0107,0x0000,0x08,0x0008,0x50,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3330,3335,3335,3340,13378,13435,0,0,0,0,0,0,0,0,0,0,19.9,19.5,19.3,19.3,-53.5,19.5,-273.2,19.5,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,19.5,18.8,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,21,832,696,704,624,0,0,1,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,1,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1223,SUCCESS 44,2023-02-02 13:28:25,220.021,0x0107,300,10,0x6001,0,65535,65535,1,19.5,13340,0,0,1,97,105,10928,11372,65535,65535,65535,2500,14400,0x00C0,1,-32767,-24018,-32767,-21000,100,0x0107,0x0000,0x08,0x0008,0x50,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3331,3336,3334,3340,13379,13435,0,0,0,0,0,0,0,0,0,0,19.8,19.5,19.3,19.3,-53.4,19.5,-273.2,19.5,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,19.5,18.8,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,25,832,696,704,624,0,0,1,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,1,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1225,SUCCESS 45,2023-02-02 13:28:30,225.022,0x0107,300,10,0x6001,0,65535,65535,1,19.5,13341,0,0,1,97,105,10928,11372,65535,65535,65535,2500,14400,0x00C0,1,-32767,-24018,-32767,-21000,100,0x0107,0x0000,0x08,0x0008,0x50,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3332,3336,3335,3340,13377,13434,0,0,0,0,0,0,0,0,0,0,19.9,19.5,19.3,19.3,-53.3,19.5,-273.2,19.5,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,19.5,18.8,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,30,832,696,704,624,0,0,1,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,1,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1230,SUCCESS 46,2023-02-02 13:28:35,230.022,0x0107,300,10,0x6001,0,65535,65535,1,19.5,13341,0,0,1,97,105,10928,11372,65535,65535,65535,2500,14400,0x00C0,1,-32767,-24018,-32767,-21000,100,0x0107,0x0000,0x08,0x0008,0x50,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3332,3336,3334,3340,13379,13433,0,0,0,0,0,0,0,0,0,0,19.9,19.5,19.3,19.3,-53.5,19.5,-273.2,19.5,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,19.5,18.8,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,35,832,696,704,624,0,0,1,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,1,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1258,SUCCESS 47,2023-02-02 13:28:40,235.293,0x0107,300,10,0x6001,0,65535,65535,1,19.5,13340,0,0,1,97,105,10928,11372,65535,65535,65535,2500,14400,0x00C0,1,-32767,-24018,-32767,-21000,100,0x0107,0x0000,0x08,0x0008,0x50,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3330,3335,3335,3340,13378,13436,0,0,0,0,0,0,0,0,0,0,19.9,19.5,19.3,19.3,-53.4,19.5,-273.2,19.5,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,19.5,18.8,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,40,832,696,704,624,0,0,1,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,1,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1204,SUCCESS 48,2023-02-02 13:28:45,240.023,0x0107,300,10,0x6001,0,65535,65535,1,19.5,13339,0,0,1,97,105,10928,11372,65535,65535,65535,2500,14400,0x00C0,1,-32767,-24018,-32767,-21000,100,0x0107,0x0000,0x08,0x0008,0x50,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3332,3335,3334,3340,13378,13435,0,0,0,0,0,0,0,0,0,0,19.9,19.5,19.3,19.3,-53.4,19.5,-273.2,19.5,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,19.5,18.8,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,45,832,696,704,624,0,0,1,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,1,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1193,SUCCESS 49,2023-02-02 13:28:50,245.024,0x0107,300,10,0x6001,0,65535,65535,1,19.5,13340,0,0,1,97,105,10928,11372,65535,65535,65535,2500,14400,0x00C0,1,-32767,-24018,-32767,-21000,100,0x0107,0x0000,0x08,0x0008,0x50,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3332,3335,3335,3340,13379,13434,0,0,0,0,0,0,0,0,0,0,19.9,19.5,19.3,19.3,-53.4,19.5,-273.2,19.5,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,19.5,18.8,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,50,832,696,704,624,0,0,1,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,1,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1179,SUCCESS 50,2023-02-02 13:28:55,250.025,0x0101,300,10,0x6001,0,65535,65535,1,19.5,13338,-57,-49,1,97,105,10928,11372,11305,13381,65535,2500,14400,0x00C0,1,-32767,-24077,-32767,-21000,100,0x0101,0x0000,0x08,0x0008,0x40,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3314,3335,3334,3340,13378,4,-1183,4,4,-11,-392,1,1,-4,-77,-66,19.9,19.5,19.3,19.3,-53.3,19.5,-273.2,19.5,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,19.5,18.8,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,2,832,696,704,624,0,0,1,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,1,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1241,SUCCESS 51,2023-02-02 13:29:00,255.311,0x0107,300,10,0x6001,0,65535,65535,1,19.7,13340,0,0,1,97,105,10928,11372,65535,65535,65535,2500,14400,0x00C0,1,-32767,-24020,-32767,-21000,100,0x0107,0x0000,0x08,0x0008,0x50,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3330,3335,3335,3340,13379,13434,0,0,0,0,0,0,0,0,0,0,19.8,19.7,19.3,19.3,-53.3,19.7,-273.2,19.7,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,19.5,18.8,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,2,832,696,704,624,0,0,1,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,1,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1204,SUCCESS 52,2023-02-02 13:29:05,260.025,0x0107,300,10,0x6001,0,65535,65535,1,19.8,13339,0,0,1,97,105,10928,11372,65535,65535,65535,2500,14400,0x00C0,1,-32767,-24041,-32767,-21000,100,0x0107,0x0000,0x08,0x0008,0x50,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3332,3335,3335,3340,13378,13434,0,0,0,0,0,0,0,0,0,0,19.9,19.8,19.3,19.3,-53.4,19.8,-273.2,19.8,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,19.5,18.8,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,7,832,696,704,624,0,0,1,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,1,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1209,SUCCESS 53,2023-02-02 13:29:10,265.026,0x0107,300,10,0x6001,0,65535,65535,1,19.8,13339,0,0,1,97,105,10928,11372,65535,65535,65535,2500,14400,0x00C0,1,-32767,-24041,-32767,-21000,100,0x0107,0x0000,0x08,0x0008,0x50,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3332,3335,3335,3340,13378,13434,0,0,0,0,0,0,0,0,0,0,19.9,19.8,19.3,19.3,-53.4,19.8,-273.2,19.8,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,19.5,18.8,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,12,832,696,704,624,0,0,1,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,1,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1241,SUCCESS 54,2023-02-02 13:29:15,270.026,0x0107,300,10,0x6001,0,65535,65535,1,19.8,13339,0,0,1,97,105,10928,11372,65535,65535,65535,2500,14400,0x00C0,1,-32767,-24041,-32767,-21000,100,0x0107,0x0000,0x08,0x0008,0x50,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3332,3335,3335,3340,13378,13436,0,0,0,0,0,0,0,0,0,0,19.9,19.8,19.3,19.3,-53.5,19.8,-273.2,19.8,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,19.5,18.8,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,17,832,696,704,624,0,0,1,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,1,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1176,SUCCESS 55,2023-02-02 13:29:20,275.310,0x0107,300,10,0x6001,0,65535,65535,1,19.8,13340,0,0,1,97,105,10928,11372,65535,65535,65535,2500,14400,0x00C0,1,-32767,-24041,-32767,-21000,100,0x0107,0x0000,0x08,0x0008,0x50,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3330,3335,3335,3340,13377,13434,0,0,0,0,0,0,0,0,0,0,19.9,19.8,19.3,19.3,-53.4,19.8,-273.2,19.8,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,19.5,18.8,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,22,832,696,704,624,0,0,1,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,1,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1204,SUCCESS 56,2023-02-02 13:29:25,280.027,0x0107,300,10,0x6001,0,65535,65535,1,19.8,13339,0,0,1,97,105,10928,11372,65535,65535,65535,2500,14400,0x00C0,1,-32767,-24041,-32767,-21000,100,0x0107,0x0000,0x08,0x0008,0x50,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3332,3336,3335,3341,13379,13434,0,0,0,0,0,0,0,0,0,0,19.9,19.8,19.3,19.3,-53.4,19.8,-273.2,19.8,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,19.5,18.8,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,27,832,696,704,624,0,0,1,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,1,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1210,SUCCESS 57,2023-02-02 13:29:30,285.027,0x0107,300,10,0x6001,0,65535,65535,1,19.8,13340,0,0,1,97,105,10928,11372,65535,65535,65535,2500,14400,0x00C0,1,-32767,-24041,-32767,-21000,100,0x0107,0x0000,0x08,0x0008,0x50,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3332,3336,3334,3340,13379,13435,0,0,0,0,0,0,0,0,0,0,19.9,19.8,19.3,19.3,-53.4,19.8,-273.2,19.8,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,19.5,18.8,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,32,832,696,704,624,0,0,1,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,1,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1237,SUCCESS 58,2023-02-02 13:29:35,290.027,0x0107,300,10,0x6001,0,65535,65535,1,19.8,13340,0,0,1,97,105,10928,11372,65535,65535,65535,2500,14400,0x00C0,1,-32767,-24041,-32767,-21000,100,0x0107,0x0000,0x08,0x0008,0x50,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3332,3336,3334,3340,13377,13435,0,0,0,0,0,0,0,0,0,0,19.9,19.8,19.3,19.3,-53.3,19.8,-273.2,19.8,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,19.5,18.8,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,37,832,696,704,624,0,0,1,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,1,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1252,SUCCESS 59,2023-02-02 13:29:40,295.314,0x0107,300,10,0x6001,0,65535,65535,1,19.8,13340,0,0,1,97,105,10928,11372,65535,65535,65535,2500,14400,0x00C0,1,-32767,-24041,-32767,-21000,100,0x0107,0x0000,0x08,0x0008,0x50,0x0014,0x0298,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3330,3335,3335,3340,13379,13434,0,0,0,0,0,0,0,0,0,0,19.9,19.8,19.3,19.3,-53.4,19.8,-273.2,19.8,10928,13754,11372,14338,11066,10928,13754,444,584,11372,14338,19.5,18.8,1000,1000,1000,1000,0,0,0,0,1,14,1,1,1,1,42,832,696,704,624,0,0,2,0,0,0,0,11658,11651,11668,11661,0,0,0,0,0,2,1.17,860,832,696,704,624,0,49858,46774,65535,832,696,704,624,16384,11527,14803,1252,SUCCESS
Best regards
Christian Rump
Hello Christian,
I looked through the log and I don't see any of the protections being set. Can you change your sampling rate to 1s intervals so we can see exactly when they get set if they do? You can also disable logging for certain registers so it can ready only VIT data with the safety and alert registers,
You can disable logging for all registers then select the ones you want by double clicking the log button:
Can you also enable the lifetime logging and then click the LT_FLUSH command after the test before exporting the .gg file an sharing?
I can't tell which hardware protection is getting triggered and the log isn't showing any protection triggered. It is strange it resets every 1s, this is how often the firmware updates all the registers.
Sincerely,
Wyatt Keller
Hello Wyatt,
Attached is the log file from the last short circuit test.
The query interval was set to 500ms.
Also included in the appendix is a watch log with a log time of 250ms with the 4 registers:
Battery Mode, Operation Status A, Safety Alert A+B and Safety Status A+B.
Data Log TimeStamp,Battery Mode,Operation Status A,Safety Alert A+B,Safety Status A+B 2023-02-06 08:56:49.310,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:56:50.402,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:56:51.528,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:56:52.655,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:56:54.232,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:56:55.359,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:56:56.480,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:56:58.010,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:56:59.121,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:57:00.247,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:57:01.834,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:57:02.965,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:57:04.076,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:57:05.643,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:57:06.730,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:57:07.843,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:57:08.996,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:57:10.587,0x6001,0x0101,0x0000,0x0000 2023-02-06 08:57:11.778,0x6001,0x0101,0x0000,0x0000 2023-02-06 08:57:12.898,0x6001,0x0101,0x0000,0x0000 2023-02-06 08:57:14.448,0x6001,0x0101,0x0000,0x0000 2023-02-06 08:57:15.604,0x6001,0x0101,0x0000,0x0000 2023-02-06 08:57:16.843,0x6001,0x0101,0x0000,0x0000 2023-02-06 08:57:18.469,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:57:19.670,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:57:20.765,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:57:22.281,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:57:23.405,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:57:24.513,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:57:26.125,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:57:27.280,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:57:28.436,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:57:29.982,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:57:31.060,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:57:32.187,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:57:33.717,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:57:34.904,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:57:36.106,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:57:37.514,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:57:38.622,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:57:39.520,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:57:40.622,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:57:42.122,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:57:43.248,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:57:44.418,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:57:45.933,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:57:47.042,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:57:48.197,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:57:49.713,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:57:50.883,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:57:52.010,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:57:53.516,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:57:54.607,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:57:55.776,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:57:56.948,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:57:58.480,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:57:59.589,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:58:00.732,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:58:02.332,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:58:03.497,0x6001,0x0101,0x0000,0x0000 2023-02-06 08:58:04.775,0x6001,0x0101,0x0000,0x0000 2023-02-06 08:58:06.354,0x6001,0x0101,0x0000,0x0000 2023-02-06 08:58:07.525,0x6001,0x0101,0x0000,0x0000 2023-02-06 08:58:08.679,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:58:10.321,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:58:11.524,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:58:12.652,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:58:14.246,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:58:15.354,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:58:16.444,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:58:18.074,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:58:19.212,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:58:20.353,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:58:21.947,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:58:23.059,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:58:24.149,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:58:25.719,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:58:26.834,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:58:27.999,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:58:29.564,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:58:30.636,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:58:31.790,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:58:32.901,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:58:34.400,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:58:35.526,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:58:36.685,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:58:38.275,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:58:39.497,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:58:40.636,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:58:42.136,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:58:43.371,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:58:44.480,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:58:46.003,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:58:47.119,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:58:48.291,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:58:49.807,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:58:50.994,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:58:52.135,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:58:53.672,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:58:54.746,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:58:55.871,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:58:57.042,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:58:58.620,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:58:59.806,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:59:00.960,0x6001,0x0101,0x0000,0x0000 2023-02-06 08:59:02.492,0x6001,0x0101,0x0000,0x0000 2023-02-06 08:59:03.617,0x6001,0x0101,0x0000,0x0000 2023-02-06 08:59:04.839,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:59:06.465,0x6001,0x0101,0x0000,0x0000 2023-02-06 08:59:07.621,0x6001,0x0101,0x0000,0x0000 2023-02-06 08:59:08.731,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:59:10.337,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:59:11.462,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:59:12.604,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:59:14.230,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:59:15.385,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:59:16.573,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:59:18.169,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:59:19.336,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:59:20.446,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:59:22.073,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:59:23.180,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:59:24.326,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:59:25.867,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:59:26.998,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:59:28.088,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:59:29.626,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:59:30.717,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:59:31.827,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:59:33.014,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:59:34.559,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:59:35.907,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:59:37.625,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:59:38.750,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:59:40.079,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:59:41.547,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:59:42.592,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:59:43.873,0x6001,0x0107,0x0000,0x0000 2023-02-06 08:59:45.115,0x6001,0x0107,0x0000,0x0000
I also activated Lifetime logging before the test and executed the LT_Flush command after the test and exported the data.
Thank you for your support
Best regards
Christian Rump
Hello Christian,
thank you for providing the additional data.
Let me take a closer look at it and respond within the next couple days, I am currently traveling and don’t have good internet.
Sincerely,
Wyatt Keller
Hello Christian,
Sorry for the delay, I have been traveling and training the last few days.
I took a look at the files shared, it looks like the lifetime data may not have properly been saved, it looks like they are still default.
Also in the logs I don't see any of the safety flags trigger, which is really strange to me. I think you have actually disabled the ASCD and ASCC protection since the enabled protections B has been modified from default. Both bits 0 and 2 should be 1, RSVD bits shouldn't be modified.
From what I can tell the gauge may not have actually registered the hardware fault because it was disabled in firmware, so on the next firmware check of the AFE registers it constantly clears the AFE fault which is why it happens every 1s in your tests.
Sincerely,
Wyatt Keller
Hello Wyatt,
yes that was the right hint.
The Reseved Bits 0 and 2 of "Settings.Protections B" were set to 0.
After the bits were set to 1, the activation only came after the time set under Protections.ASCD.Recovery. (Actually after 10sec)
Thank you for your support.
Best regards
Christian Rump