This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
BQ40Z50-R1 Latch count configuration is valid once, but if invalid multiple times, can it be configured to lock after triggering three short circuits.
Hi Shirish,
I set it three times to trigger, but not short-circuit it three times to trigger the latch. Are there any other parameters need to be set ?
Yes, please refer the TRM
The thresholds are in section A.3 Short Circuit in Discharge (ASCD1 and ASCD2)