This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS26630-33EVM: PGOOD vs latching overcurrent protection.

Part Number: TPS26630-33EVM

I am having some trouble getting the TPS26631 to perform as expected.

I am using the device as input protection for a device and have the following requirements:
reverse polarity preotection, uvlo (9V), ovlo (30V), overcurrent protection (3.8A, latch-off).
Furthermore I have the PGOOD configured to trigger at 8.5V and tied to the enable of the SMPS.

I am using the demoboard to prototype this (with 600mA current limit).
However, I am running into the following issue. 

When the load reaches 600mA, the output voltage of the TPS26631 starts to drop, when it reaches 8V, the PGOOD goes low.
This in turn causes the SMPS to switch off and the load to disappear, the TPS recovers and the whole thing starts again.
This causes the output of the TPS26631 to go into a hiccup mode instead of latching off.


Yellow: Input Voltage
Blue: Output Voltage
Green: Output Current
Red: PGOOD


What should I change in order to fix this?

  • Hi Richard,

    Thanks for reaching out!

    The eFuse devices latches-off during overcurrent event if the overcurrent event causes enough power stress to trigger thermal shutdown.

    The FLT/ goes low for overcurrent event, use that information to pulldown the SHDN/ pin to latch-off the eFuse

    Best Regards,

    Rakesh