Hi Team,
Can you help clarify the question below?
According to the datasheet, the shutdown current of the TPS61088 is 3uAn measured when no load and no feedback resistor divider is connected.
If the design has a load and feedback resistors to be connected during the shutdown. What is the current of VIN during shutdown (EN=0V) if load and feedback resistors are connected? Or is VOUT=VIN in shutdown?
Thank you.
Regards,
Marvin