Hello TI Team,
I am trying to enter into sleep mode in BQ7695202 when the DFET is control off by DFETOFF pin. I have also set the necessary registers according to the attachment.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello TI Team,
I am trying to enter into sleep mode in BQ7695202 when the DFET is control off by DFETOFF pin. I have also set the necessary registers according to the attachment.
The following is the sleep state of the battery when the DFETOFF is pulled low and the DFETOFF is high
the left figure shows the bq76952 active when the DFETOFF is not pull down, the right one show the bq7695202 sleep when the DFETOFF is pull down.
Hi Sheng,
I tested this on my board. You are correct, disabling the discharge FET with the DFETOFF pin does prevent the device from going into SLEEP mode. If you disable the DSG FET with the DSG_PDSG_OFF() command, it will not prevent SLEEP mode, so this might be a better option for you.
Best regards,
Matt