This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50: BQ40Z50: Battery Gauge : RemCap > Design Capacity

Part Number: BQ40Z50
Other Parts Discussed in Thread: BQ24610

The Design Capacity of BQ40Z50 is 13,000mAh.

RemCap (Remaing Capacity) and FCC (Full Charging Capacity ) were less than 12,000mAh.

When I raised the charging voltage, sometimes RemCap and FCC exceeded 13,000mAh.

After VCT flag, the BQ40Z50 adjusts the RemCap and FCC below 13,000mAh.

Question : 

    Is it problem if RemCap and FCC are higer than Design Capacity ? 

    Does it okay if it is compensated ? 

     

  • System
    • Battery Gauge : BQ40Z50.
    • Battery : 2S3P, 14,700mAh.
    • Charger : BQ24610.