Hello Ti Team,
We are seeking for support, in order to detect devices on the GUI.
The first problem is that the GUI doesn't detect devices from the EVM and show this error: "Connected to AEVM Controller, but failed to connect to device TPSG694x_2p0_external on DUTWITHI2C @0x48"
- V3V3 and V_SYS are connected on J15, the card is powered by USB, moreover D4, D5,D6 are on, whereas D3 is off.
- We measure VCCA, we get 0V. -> PMIC doesn't answer on the I2C bus because of this, right ?
- On J15, pin 6 VSYS_SENSE, we get 0V. -> We think that VCCA is at 0V because of this.
- Testing on R21, we get 3.3V
- Testing on R39, we get 5V (very weird). But we suspect that R39 is maybe wrong named because it's placed far from R20 and R21.
.
- There is none R27, on the board.
Thank you in advance for your help,
AB