Other Parts Discussed in Thread: LM5170
Hi,
I am trying to use LM5170 EVM-BIDIR, in buck mode. I am able to produce the desired voltage when load is not connected (open circuit) but once I connect the load at the LV side, the voltage reduces to very low value of 0.13V. I am giving the PWM and the master enable using TI C2000 TMS F28379D. I have made all the connections as per the user manual, but I am not able to figure out what I am doing wrong. I have attached the board connection that I am using. Can you please help me out with this?
Thanks.