Hi, Support Team
We have some question for bin file read/write to EEPROM
Q1:What’ the default status of GPIO0, input/output?
Q2:Plan to use TPS25762-Q1 GPIO0 for control the TVSP index selection between 0 to 5 ,Could GPIO0 control by I2C1 register from MCU in runtime?
Q3:Could TPS25762-Q1 boot up without EEPROM bin?
Q4 :TPS25762-Q1 boot up steps for confirm, is correct?
a .EEPROM empty
b.TPS25762-Q1 boot up mode select to index 0 (but the EEPROM is empty)
c.GPIO0 set from low to high via I2C1 from MCU
d.Send bin file from MCU to TPS25762-Q1 to EEPROM
e.GPIO0 set from high to low via I2C1 from MCU
f.TPS25762-Q1 boot up mode index 0 (EEPROM with bin)
schematic:
if any suggestion, Please advise me.
Thanks,
Best regards,
Lawrence