Hello,
I have BQ76952 AFE with which I've been able to test passive balancing during relaxation with bleed resistor value being 41 ohm(Did add 6 parallel resistors for the cell with max voltage so that dissipation is quick). When I do the balancing during charging, I'm seeing one of the cell quickly hitting over voltage threshold & hence balancing stops. I had the charging current tried with 3A, 0.5A. I had the same problem. Balancing while charging seems to work fine if I have 0.05A for the charging current which I wouldn't prefer doing.
Battery chemistry: Lithium Ferrous phosphate
Battery capacity: 6Ah, nominal cell voltage 3.3V; My test setup actually has 2 AFE with each connecting to 12 cells. Cell mapping has already been done and verified with TI.