This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV62569: A ringing problem occurs.

Part Number: TLV62569

Hi,

We are using TLV62569DBV to achieve 5V to 3.3V.

Design schematics and oscilloscope test drawings are shown in the attached documents.

I have two questions, please help to reply:

1. Is the ripple of output Power supply in Power Save Mode Operation larger than that in ordinary PWM operation?

2. How to disable TLV62569DBV from entering the Power Save Mode Operation mode? Most application scenarios are not sensitive to power consumption.

TLV62569DBV.docx

Thanks a lot !