Other Parts Discussed in Thread: LMG2610, , LMG5200, LM76005
Hello:
ds for LMG2610 states that the part is meant for a[[lications <75W
Yet, nowhere can one notice where that limit comes from.
Surely, one place would be the input voltage limit: the lower it is, the higher the peak current and perhaps lower Lm also forces higher leakage thus causing higher upper GaN peak currents.
In order to satisfy the 100W limit offered under the USB C PD and adopters, it is safe to specify that the lowest input level will be 120V, not 100V.
Will that exceed any SOA boundaries?
Any comments on this will be highly appreciated..
R