This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi guys,
Could I please get copy of the original project file [.pjt] for the TUSB1146EVM?
Out of the box, only the USB works as expected, though the DP detection does not work.
After debugging into the EVM via Aardvark, I can see that the DP Alt Mode / PD negotiations aren't even configured.
While I'm at it, could I please get the original project files for:
TSUB546EVM
TUSB1046EVM
TUSB564RNQEVM
TUSB1064RNQEVM
Kind regards,
Jack.
Hi Brain,
I mean, the project/configuration file for the TPS65987D controller (for the TUSB1146EVM case), mounted on the EVM.
Kind regards,
Jack.
Jack:
project file should be loaded to PD controller when board as build.
Regards
Brian
Brain:
Yes, you're correct, they are loaded onto the PD controller when the board is built;
though I'm going to be loading custom configurations onto the device to test non-default functionalities, and would like a copy of the stock project files to return the device to its default state once I'm done testing.
Kind regards,
Jack.
Please see link below.
https://tidrive.itg.ti.com/a/XBe170KXtftOF7Xl/75c971ae-31cb-44c4-a116-164d2253416c?l
Hi Undrea,
I cannot access it; I imagine because it is restricted to TI employees?
Kind regards,
Jack.
Hi Undrea,
Thank you very much, I've downloaded the two files:
- TUSB1146EVM_Release.bin
- TUSB1146EVM_Release.pjt
Is this the configuration of the TPS65987D mounted on the TUSB1146EVM?
If it isn't, do I require a separate software/GUI to configure the TUSB1146 device?
For reference, I've been using "TPS65981_2_6_7_8 Application Customization 6.1.3" for the TPS65987D.
Lastly, to save time having to open a new E2E thread and request each of the following, individually. May I please also get the files via BOX for:
TSUB546EVM
TUSB1046EVM
TUSB564RNQEVM
TUSB1064RNQEVM
We are testing all of these solutions in parallel.
Kindest regards,
Jack.
TUSB546/1046 EVMs share the same PD controller firmware, same for TUSB564/1064. Please see link below:
https://txn.box.com/s/l4i4tp9f67dg9ylcqt3ykkjqn5djlc5n
Regards,
Undrea