This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40428: Questions about the TPS40428

Part Number: TPS40428

I am using TPS40428 in a design and I have some questions.

  1. I couldn't find anywhere in the datasheet that it's written explicitly what is the maximum current the converter can supply when operating in 2-phase mode (when using the recommended power stages).
  2. The datasheet says the current limit default configuration is 40A but after testing it's seems like 30A.
  3. What is the right way to make the converter work with 60A current. The maximum current limit that can be configured is 50A. I found the IOUT_CAL_GAIN that can be set higher to get a higher current limit.
  4. Continuing the previous question, can the current limit just be cancelled? I don't need it and it's just disturbing.
  5. Summary question- I want to work with TPS40428 in the next conditions:
    a. Smart Power Mode
    b. 60A output current
    c. 0.85V output voltage
    d. No current limit
    e. I'd like not to have to configure the component digitally but only with hardware. If not possible I'd like to know the simplest way to configure it.

Note- The current design is attached.TPS40428_RAFAEL.pdf