Part Number: PTD08D210W
Other Parts Discussed in Thread: UCD9248, , UCD9224EVM-464
Hello,
I use the software FUSION DIGITAL POWER DESINGER and I got a problem in the monitoring window, the output current is not corresponding to the real current.
I have a UCD9248 and a PTD08D210 components on the board.
I put a variable load at the output and an ampere meter to see in real time the value of the current.
If I modify the values of the Iout cal gain and Iout cal offset, this change the value of the current on the monitoring.
Even if I modify this two parameters to have the same current on the amperemeter and the monitoring, this is valid only for this current because if I modify the charge value, the current on the amperemeter and the monitoring are differents.
The evolution of the current on the amperemeter is in correlation of the current in the datasheet of the ptd08d210W page8 figure19.
Is-there a parameter or a specific configuration to have to observe the current in real time on the system monitor?
If you want some specification or screenshot don't hesitate.
Thanks in advance,
Maxime