This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Brian,
Could you provide more information about the following items?
Could you also share some more information about customer's application which needs these requirements?
Thank you.
Regards
Lei
Hi Lei,
1.The Vin can be 1-6V.
2.Max Vout >15V is OK.
3.max Iq=1uA.
4.max soft start time = 1ms
It is used for back clamped ultrasonic flowmeter.
So they need fast soft start time to rapidly response for the ultrasonic test, and also they need low Iq to achieve a low power comsumption.
Best Regards,
Brian
Hi Brian,
Currently TPS61096A will be the most suitable option for the descripted application, and no newer version yet.
If customer required max 1ms ss time and can't accept typ 1mm ss time, then need to look for other options.
Regards
Lei