This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5118: problem with HO signal

Part Number: LM5118

Hello good morning
I have a noise problem with the HO pin switching signal.
The signal looks like this:

VIN = 24VDC.

VOUT = 12VDC.

switching frequency = 100 KHZ.

I don't have load for the output.

This is my circuit, I got it from webench power designer

thank you very much in advance, I would be very pleased if you could help me.