This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Can we use LM25116MH/NOPB IC in CC/CV mode?
For my design I need both current and voltage controlled IC like LM5117. Is this LM25116MH/NOPB suitable?
What is different between LM25116 and LM5148 IC? Which one is better option for CC/CV mode and better duty cycle?
Hello Ramaprasad
Unfortunately, LM25116 doesn't provide the current monitor function like as LM5117. You have to use an externa circuit if you'd like to achieve CCCV using LM25116 or LM5148.
Also, LM25116 doesn't support the low dropout operation which LM5148 supports. Please create a new post if you have a question about LM5148.
- EL