Hi Team,
Can you have a look at the following customer inquiry, please? I can provide a schematic offline, if needed.
We are using a number of different TI boost converters in a new pump design. However, we are encountering a serious failure of the TPS61088 during our initial bring-up.
The failure appears to be shorting out (8 ohms to GND) ) of SW outputs of the device at power-up. The max current we need is ~100ma @ Vin=5V , VOUT 9V. We have the device set for PFM mode using 2.2uH uH 1A inductor.
We did not take any oscilloscope measurements because the failure either was before enabling Vin (possible bad part) or immediately after applying Vin.
- While applying Vin there was no load on Vout.
- The output capacitors were disconnected by a jumper as well.
We have reviewed the TI knowledge base for similar issues and found some evidence of layout, but no mention of the specific reason. We have reviewed and components values, manufacturing issues along with the layout.
- https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/588165/tps61088-tps61088
- https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/588086/tps61088-ic-is-damaged-when-loaded-with-ptn78000a
At first we suspected some defective devices or poor soldering. However I’m not sure. My suspicion of a ‘possible’ issue was the reviewing of e2e reporting similar events.
Once we replaced the device(s) from a different lot we did take some A/B comparisons (original design versus new design –layout only) of the inductor current. The failure appeared to be shorted (8 ohms) on all the SW pins. I’m thinking or speculating that our placement of the output caps may not be optimal or the inductor. So really I’d like to understand what the possible failure mechanism(s). Could having no output caps connected cause this failure? or some added inductance. We removed TP306 during initial debug (no load).
We now have one board that is working with no changes or fixes implemented (just new device installed). We are few days away from receiving more boards and want to be better prepared if the issues arises again.
Thank you,
Franz