We have Vin 22-32V and Vout 20V 100mA.
Currently we are using LMS3655 in a flybuck mode.
I dont understand why there is LM61460 as a suggestion and described as "lower EMI" when the datasheet shows better EMI with the LMS. Can you explain?
We barely passed our automotive customers conducted emissions with alot of work and filtering components, but i am regretting for not going for some adjustable frequency controller instead, such as or a ZVS ucc28781 which selects frequency based on the inductance which we could have had large. It can operate in audible frequency at low loads and 100mA is still a low load. Only the 10th or so harmonic would start at the 150kHz which is where conducted EMI starts to be measured. Easy pass. Do you agree?