This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I'm trying to adjust the output of the TPS548B28EVM-023 evaluation module to 3.30V. According to section 1.3.1 on page 3 of the TPS548B28EVM-023 User Guide, the Output Voltage Setpoint is: (R6+R7) = [(Vout-Vintref)/Vintref] x 10000.
Assuming:
Vintref = 0.60
R7 = 0 ohms
R6 = 45300 ohms
Vout should work out to 3.318V but I'm measuring a much lower value, around 3.01V.
What am I doing wrong?
Can you recommend the correct R6 value?
Thanks.
Hello Bill,
try using 10K on top and 2.5K on the bottom or any other combination that can give 3.0V
thanks
Tahar
Hi Bill,
Were you able to get 3.3V output on the TPS548B28EVM
Hi David,
I don't know if you can see it but this is what I replied to Tahar:
Hello Tahar,
1. I need the output to be 3.3V, not 3.0V.
2. To avoid any confusion, please specify which resistor is on top. Is it R6 or R9? If I define R6 as 2.5K and R9 as 10K, the equation produces an output value of 0.75V.
I have attached the schematic for your reference.
Thanks,
Bill
Hello Tahar,
1. I need the output to be 3.3V, not 3.0V.
2. To avoid any confusion, please specify which resistor is on top. Is it R6 or R9? If I define R6 as 2.5K and R9 as 10K, the equation produces an output value of 0.75V.
I have attached the schematic for your reference.
Thanks,
Bill
R9 = 10kOhm (low side feedback resistor)and R6+R9 = 45.3kOhm should yield an output voltage of 3.3V.
If you are using 10k and 45.3k resistors and getting a 3.0V on the Vout+ and Vout- test point, can you check the SW node test point with respect to PGND using an oscilloscope. The SW should be a periodic pulse train with pulses that have consistent pulse widths.
Also, check the SS/REFIN pin voltage with wrt to AGND and make sure voltage is greater than 0.6V.
During your test what is the input voltage and output current
Hello Tahar,
I'm now getting the correct voltage output of 3.324V. I have no idea why I didn't get the same result earlier. Very strange. Anyway, thanks for your assistance. We can close this case now.
Thanks,
Bill
Hi David,
I'm now getting the correct voltage output of 3.324V. I have no idea why I didn't get the same result earlier. Very strange. Anyway, thanks for your assistance. We can close this case now.
Thanks,
Bill
Thanks for the update and I will close. If the incident repeats, post the issue again and let's root cause
Best Regards,
David