This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I plan to use LM2585 to convert input 24V to 300V. In WE bench I have got the simulation results which is shown below. I have a query regarding transformer ratio.
In the BOM the transformer specification is mentioned as below:
Ns1toNp: 10 Lp: 485.11 µH Leakage_L: 9.7 µH
Does this mean secondary turns is less than primary turns by a factor of 10?
since this is a boost application, the secondary turns must be higher than primary turns right.
Please let me know if I am right.
Hello Vijan,
Thanks for reaching out to us via e2e.
You are right, the number of the output windings has to be 10x the number of input windings.
And I agree that this notation can be misleading.
You could have multiple secondary windings, e.g. for different output voltages.
Therefore, the outputs are numbered: secondary #1 (s1), secondary #2 (s2), ...
So, this notation means:
number of windings for secondary #1 to number of windings for primary: 10
Please be careful with the orientation of the output winding, to connect the diode to the correct terminal of the transformer.
Best regards
Harry
Hi Harry,
Thank you for the detailed explanation. This sure helps :)
Best regards
Vijay