This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
Does it have output capacitor limitation? 8.2.2.3.2 Output Capacitor C2 shows just minimum capacitance. Does it have maximum allowable output capacitance?
Is there any concern for VOUT=5V when VIN=EN=0V? How much current does this device sink into OUT from 5V?
Regards,
Ochi
1. wE DON'T ;IMIT THE MAXIMUM CAPCITANCE, BUT if the Cout too large, due to package, the esr may be large as well, which adds to the output ripple as well . Also the zero yielded by Cout and esr may be lower, which doesn't mean the lower the better .
2.The typical value is 50nA , refer to table
Hi Yoshiki,
I noted that this is a auto application, we have a new 5V output auto device TPS61033x-Q1 (sample now, RTM in 3Q), I think maybe TPS61033x is a better option, TPS61071-q1 is very old device...
Do we have changes to promote TPS61033x? Please make us know if customer is interested in this new devices. Thanks.
Regards,
Nathan