Other Parts Discussed in Thread: USB2ANY, LP8864EVM
excuse me if appear above picture how can i do
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, wade
It means that you don't update USB2ANY correctly, pls follow the step and update the USB2ANY
so how can i do?
MODE 5xx USB
RX_PASSWORD pass32_wrong.txt
RX_PASSWORD pass32_default.txt
RX_DATA_BLOCK_FAST RAM_BSL_USB.txt
SET_PC 0x2504
DELAY 4000
MODE 5xx USB
RX_PASSWORD pass32_default.txt
RX_DATA_BLOCK myflash.txt
RX_DATA_BLOCK poststep1.txt
RX_DATA_BLOCK poststep1.txt
Hi, Wade
You need to make sure computer connected with USB2ANY first. You can try a software called USB2ANY EXPLORE.
Hi Wade,
Please try to updating the firmware just to 2.8.2.0 using the standalone SDK firmware updater binary in below link:
After installing the SDK, you can locate the firmware updater binary in C:\Program Files (x86)\TI USB2ANY SDK\bin\USB2ANY Firmware Loader.exe.
Once USB2ANY is on 2.8.2.0 firmware, it should be easier to update to the next revision.
Best Regards,
Jared
Hi Wade,
Please hold the BSL button and then try to launch the USB2ANY Firmware Loader.exe.
BR
Jared
Hi Wade,
You just need to a USB2ANY and connect it to your notebook. No EVM board is needed, only notebook and USB2ANY are needed. After updating to 2.8.2.0, you can use the GUI to update the new version.
BR
Jared
Hi Wade,
Please hold the BSL button and click the "yes" button to install 2.8.2.0.
Hi Wade,
Please follow the instructions. You need to unplug and plug the USB port while holding the BSL button.
BR
Jared
Hi Wade,
Glad to help you, our AE zhiqian will support the specific case of this device later.
Thanks and best regards,
Jared
Hi, wade
Pls see the user guide of LP8864EVM, you can find it in the ti website.