Other Parts Discussed in Thread: PMP6812, TPS23754,
1.电感L1的作用是什么,是必需的吗?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Runtao,
Hope you do not mind, but E2E uses English to communicate.
In the picture you have circled L3,
its purpose is to act as the output inductor of the active clamp forward DC/DC converter. It is needed as a component of the forward converter to store energy.
If you want to use a flyback converter, which does not have this output inductor, I would advise looking at the TPS23754EVM-420 EVM instead.
If you are asking about L1, it is acting as a low-pass pi filter.
Let us know if you have further questions,
Sarah
Hi Runtao,
May I know what transformer you are using at U49?
I am not familiar with this EP_T838S, and cannot find any information on it, but it appears to be a forward converter.
Could you send the datasheet for this component, if able?
It seems as though most of your connections on the secondary side are still for a forward topology,
you will need to adjust these for flyback topology.
PMP6812 is a reference design for the TPS23754 using flyback topology for a 12V output:
https://www.ti.com.cn/tool/cn/PMP6812
This schematic could be a better reference suited to your needs.
Thank you,
Sarah
Hi Runtao,
Yes, that is true. If you want the higher efficiency of the TPS23754EVM-383 design, then you will have a forward topology, since it has a forward converter design.
And so you will need to implement the L3 capacitor which you first asked about, and follow the rest of the connections depicted in the EVM schematic.
Best,
Sarah
Hi Sarah,
Thanks for your replay.For higher conversion efficiency, active forward clamping will be used.Could you please help check the circuit?
Another thing, can I make some adjustments when referring to the design of TPS23754EVM-383? The VCC input uses flyback mode, and other places refer to TPS23754EVM-383.
Hi Sarah,
The response regarding 'Another thing, can I make some adjustments when referring to the design of TPS23754EVM-383? The VCC input uses flyback mode, and other places refer to TPS23754EVM-383.' specifically refers to he following drawing.