Other Parts Discussed in Thread: UCD3138
Into production and suddenly I'm unable to program our power boards. As far as I know, the UCD3138A is unchanged (checking to verify this and get very specific part numbers).
- Board(s, we've tried 2 of 20 now and got same results)
- Board turn-on procedures as previous. UCD3138A gets proper power.
- Using the UCD3xxx Device GUI to program.
- Hit "Scan for Device in ROM mode"
| Timestamp | Message |
| 6/2/2023 3:39:17 PM | Looking for device in ROM mode at address 11d ... |
| 6/2/2023 3:39:17 PM | Reading ROM version ... |
| 6/2/2023 3:39:17 PM | SAA: BlockRead (Address 11d, Cmd 0xEC): ACK 0x00030002 |
| 6/2/2023 3:39:17 PM | Reading Dev ID Register ... |
| 6/2/2023 3:39:17 PM | SAA: BlockWrite (Address 11d, Cmd 0xFD, 0xFFFFFFF0): ACK |
| 6/2/2023 3:39:17 PM | SAA: BlockRead (Address 11d, Cmd 0xFA): ACK 0x0000547F |
| 6/2/2023 3:39:17 PM | Reading PKGID ... |
| 6/2/2023 3:39:17 PM | SAA: BlockWrite (Address 11d, Cmd 0xFD, 0xFFF7F010): ACK |
| 6/2/2023 3:39:17 PM | SAA: BlockRead (Address 11d, Cmd 0xFA): ACK 0x00000001 |
| 6/2/2023 3:39:17 PM | Found ROM v2 IC v3 - UCD3138 Rev2 |
- This is the SAME message we always had previous revisions (development and first production run).
- In "Firmware Download" interface when hitting Download after selecting file.
| Timestamp | Message |
| 6/2/2023 3:41:23 PM | USB Adapter v1.0.11 [PEC; 400 kHz] Found (Adapter #1) |
| 6/2/2023 3:41:23 PM | Looking for device in ROM mode ... |
| 6/2/2023 3:41:23 PM | Reading Dev ID Register ... |
| 6/2/2023 3:41:23 PM | ROM v2 IC v3 detected |
| 6/2/2023 3:41:23 PM | Ready to download firmware |
| 6/2/2023 3:41:27 PM | |
| 6/2/2023 3:41:27 PM | Error: The firmware selected with device id: UCD3138A is not compatible with the IC: UCD3100. Refresh version A for IC is needed.Please select another firmware file. |