Other Parts Discussed in Thread: UCD3138,
Due to acquisition problems, my company has made a production run of a power board using UCD3138RHAR in place of the previous UCD318Axxxx. This was on the advice/suggestion of TI. Although they are pin compatible, they are NOT code compatible.
I've begun trying to take the same project and build for new target. Build configuration is very similar (or is now after manipulation). I can build the code. I can program the output .x0 file using the UCD31xxx Device GUI. However, currently the code will NOT run. Simply doesn't respond to the PMBUS DEVICE_ID query and then reverts to BOOT mode (ROM Mode ID only). I can zip up the entire project at this point if someone can look through all the settings and/or initialization code and spot what is causing the UCD3138 to NOT run at all.
Please advise.