HI,
I have Designed Forward converter 240W using UCC35706, Mode1, PWM frequency 130KHz,Dmax=0.65
Input : 180V AC to 240V AC / 50Hz
Output : 24V DC / 10A
a) For purpose of testing i have connected 12V DC External supply
b) Maximum output voltage is raising only to 6V & OSC pin (RC) is resetting.
unable to measure output switching voltage / PWM frequency.
regards
M.Sreenivasan
mBil:919880037604