Input : 170 V AC to 265 V AC 50Hz
Output: 110V DC ,2A
Device Selection : ucc35706
With Flyback topology Input MOSFET becomes very HOT(Even with forced cooling),shall I go for Forward topology?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.