This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5164-Q1: PGOOD operation

Part Number: LM5164-Q1
Other Parts Discussed in Thread: LM5164

Hello,

Is the operation of the PGOOD signal as simple as:

Assuming the IC is powered.

If the voltage on the FB pin is < .9*VREF (.9 * 1.2 = 1.08V), PGood will be driven low?

If, for example, the LM5164 IC was powered and I directly hooked up a voltage source to the FB pin, would I see PGOOD toggle as I move the V_test Voltage around the PGOOD Thresholds.

A customer was concerned about PGOOD operation if the high-side switch in the LM5164 fails, does PGOOD take any other information into account, or does it only look at the FB voltage.

Thanks,

Chris