This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS3610: WDI pin function

Part Number: TPS3610

Hi.

When the WDI pin of the TPS3610 was left open, I observed a pulse with a period of about 700ms.
Is this the signal the TPS3610 outputs itself to reset the internal watchdog timer?

CH4 is the WDI pin waveform.

When I connected the WDI pin of the TPS3610 to my microcontroller, the WDI pin went to about 2.5V.
At this time, a pulse signal of about 700ms cannot be confirmed, so the internal watchdog timer should not be reset, but the TPS3610 does not enable the reset signal.
Why is this?