Part Number: TPS755
Other Parts Discussed in Thread: TPS7A53,
Hi team,
The customer would like to use TPS75533KTT for high current applications:
The output is 3.3V at an input voltage of 5V, with a voltage drop of 1.7V. Based on the maximum current of 5A in the manual, the heat power of the chip is 8.5W, which translates to a temperature rise of 328℃ (the parameter on the manual is that the bottom is not copper-coated), which has already exceeded the operating temperature of the chip. In this case, how to get the chip current to 5A? Is it all about cooling?


Could you help check this case? Thanks.
Best Regards,
Cherry