Part Number: BQ77915
Other Parts Discussed in Thread: BQ77905
Hey Luis, I have a question from the last design review
You may also have to use multiple external balancing resistors in parallel in order to handle higher currents. At 20-Ohms (Ignoring MOSFET resistance) your current external balancing resistor should be able to handle 3.6-V*0.18-A = 2 Watts of power. So that would be something else to take into account.
Regarding this statement, if 20-ohms resistor is used then the external balancing current is 3.6 V / 20 Ohms = 180 mA and the power being dissipated should be 0.18A*3.6V = 648 mW. Am i missing something here ? why would it be 2 W ?
Regards