Other Parts Discussed in Thread: TPS65988, TPS65988DJEVM, TPS65988DJ
I'm designing a docking station/hub that has one USB Type C port with 100W Power Delivery (PD) set up as a sink, and another Type C port with PD set up as a source and also requires USB 2.0 Upstream Facing Port data capability. Essentially, I need to be able to do power pass through and USB 2.0.
It looks like the TPS65988DK will be able to do the whole job of the power delivery and I can add an additional USB2 Hub Controller (TUSB2046IBVF) for the USB 2.0 hub control. It looks like the software can be preconfigured in TI's configuration tool and loaded onto an EEPROM. Am I correct in understanding that the TPS65988DK does NOT require external HOST controller (i.e. a microprocessor)?