Other Parts Discussed in Thread: TPS25730, TPS25751
Tool/software:
Hello Team,
We are going to develop a custom board based on TPS65988.
I's like to to ask whether if it possible to have the following configuration without having external MCU control or switches.
1) Port A (connect to smartphone USB-C with DisplayPort Alt Mode) :
as sink if Port B is not connected (get power and DisplayPort from smartphone to operate)
as source if Port B is connected for charging smartphone (get DisplayPort from smartphone)
2) Port B as sink only (get external power source)
Use Case 1: The device is powered from VBUS only, port A sinks, port B not connected
Use Case 2: The device is powered externally, both port A sources and B sinks
Can TPS65988 achieve the configuration above without MCU?
And is there any application note or reference design that i can refer to?
Thanks.