Hi Expert,
I want to confirm with you about the MSPI mode in BQ79371-q1.
You can see the structure shown below.
- DSP communicate with 79600 via spi
- 79600 and two 79731 form a daisy chain string
- Device1(79731) communicate with ucc5871 via SPI(Master SPI stack device mode). BQ79731 have no SPI communication with DSP
Question:
1. We can see that BQ73731 need to communicate with ucc5871 using MSPI. MSPI has 2 mode, base mode and stack mode. Only stack mode could be used on the mode right? If based mode could be used, could we confugure register to transfer the Base mode to stack mode? i didn't find the register to transfer
2. If it is convenient for you, would you mind sharing the register configuration like pseudo-code with me?
3. Is there any suggestion on the structure?
Kind Regards
Imelda