This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC256404: UCC256404

Part Number: UCC256404
Other Parts Discussed in Thread: PFCLLCSREVM034, UCC24624, UCC28064A, PMP,

Hi Mani

I am using Ref your Ref Design

PFCLLCSREVM034 User Guide

On the ref schematic (12V output )  my Output Voltage 32V@ 12.5A

Page 10 on the schematic VB connected to U1 VDD  I check the data sheet U1 it says max VDD 26V Sink current 15mA

So I  Have to  use !K ,Voltage drop is 15V. So 32V-15V=17V so I can connected VDD on U1 (UCC26624DR)

Please advice

Thanks for the help

Regards

Sam