This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TI team,
Good evening.
We have designed the buck converter using LM5143QRWGRQ1 IC with below specification
Input Voltage: 36V
Output Voltage: 24V 30A
Kindly review the circuit.
Thanking you,
M H Jayaraman.
Hello,
Can you please help fill out the LM5143DESIGN-CALC tool for this review.
Also since you referenced PMP31202 multiphase (4 phase) design I am expecting the schematic to look similar to it other than the components on FB and compensation.
Regards,
Jimmy
Hi Jimmy,
Good morning,
We modified the document as you said and attached here.
Kindly Review it.
FYI,
Our expectations :
Input: 36V
Output : 0 - 24 V 30A
If you have any other recommendations, kindly advise us.
Hello Jayaraman
Please reply with the completed quick-start (You can download at https://www.ti.com/lit/zip/SNVC229 ) as Jimmy mentioned.
-EL
Hi Eric Lee,
Good evening.
Kindly review the schematic of Buck converter using two LM5143 ICs.
Input:36V
Output:1.5V to 24V variable voltage with 30A.
We can obtain the variable voltage or not?
Thanks,
Jayaraman M H
Hello Jayaraman
Would you please reply with the completed quick-start? (You can download at https://www.ti.com/lit/zip/SNVC229 )
-EL