Other Parts Discussed in Thread: PFCLLCSREVM034, PMP22087, UCC28064A, PMP, UCC28180, UCC256404
Hi Ray
What is the good ref design that I have o follow?
I am integrating UCC28056 with UCC25640A
1. UCC28056 Data sheet schematic Page 22 or PFCLLCSREVM034 Schematic Diagram: PFC Section Page 9
My Output from UCC25640A is 32V@12.5A
I used the calculator. it calculate max out PFC
OUTPUT: | |||
Maximum Output Power of PFC Stage: | POUT | 165 | W |
Output Voltage (Note: Must be > VIN_RECTIFIED(max)): | VOUT | 390 | V |
Maximum Output Voltage Allowed Peak to Peak Low Frequency Ripple Factor (i.e. 0.02 for 2%, 0.05 for 5%). Not recommended to be > 5%: |
VOUT_ripple_factor | 0.05 | |
Maximum Output Voltage Allowed Peak to Peak Low Frequency Ripple | ΔVPPK | 19.5 | V |
Maximum Ambient Temperature: | TAMB(max) | 50 | °C |
Maximum Average Output Current of PFC Stage: | IOUT | 0.423 | A |
Minimum Equivalent Load Resistor | RLOAD | 921.8 | W |
In this case so I can use either circuit?
Please advice
Regards
Sam