Other Parts Discussed in Thread: TPS5450
In the respective circuit a 3.8V is generated from +10V input. My queries are related to the noise reduction
1. In the input rail an inductor ,capacitor combination is used. what is the purpose of that ? is it acting as a filter. Do we really want to connect such combination in the input side.
2. what should be the value of input capacitors , I have seen 4.7 uF combination at the input. can i use different capacitance ?
3. what should be the value of output capacitance?
4. How to reduce the ripple in voltage and current?
May be these are basic questions but i really appreciate if you could answer these questions.
Thanks in advance
/